Skip to main content
Jiannong Zhou
Associate III
Apr 12, 2020 10:55 AM UTC
Question

There are some issues when generate code with STM32CubeMX 5.6.1 and run the code

  1. there is a strange issue when generate a code. The code generation cannot be ended with an error - "But EWARM V8project generation have a problem. before the code can be generated without an errors.
  2. After run generated code, always be hang at SystemClock_Config(); halt on HSI_TIMEOUT_VALUE.

I have no issues for the code with the previous version 4.27.0.

Please advise on these two issues. thanks.

Regards,

Jiannong

This topic has been closed for replies.

3 replies

Nesrine.JLASSI
Visitor II
Apr 14, 2020 9:50 AM UTC

Hi @Community member​ 

Could you please share your .ioc file to check the issue ?

Regards,

Nesrine

Jiannong Zhou
Associate III
Apr 14, 2020 1:40 PM UTC

Hi Nesrine,

I already deleted not working .ioc file. Attached the working one. This new version .ioc file migrated from old version of STM32CubeMX.

There could be a possiuble reason for .mxproject. in the file, the project folder is not the current project folder.

I will share with you .ioc file when face the problem again.

Thanks & regards,

Jiannong

Nesrine.JLASSI
Visitor II
Apr 14, 2020 2:15 PM UTC

Hi @Community member​ ,

Okay, you are welcome any time :)

Best regards,

Nesrine