The instructions in UM1718 Rev 37 Chapter 15, page 292 compatible processors is running for 4 hours and is only 50% done.
- 2 replies
- 1086 views
I have STM32CubeIDE 1.9.0 and I am editing the .ioc.
In the Pinout & Configuration Tab I right click and select List Pinout Compatible MCUs
It starts runningand running and running. Last night I let it run all night and it said it was 8% and there was a red message Running Low Memory.
I rebooted the computer and reran it. After 4 hours it is at 50% and I got the Running Low Memory and it appears to have stopped.
See attached screen shot. Error1.png
My computer has 32 GB RAM and nothing else was running. The Task manager says 1,559.6 MB of memory is being used. I put the process priority from normal to above normal, and that did not make a difference. It says I am using a total of 7.2 of 31.8 GB (23%) of memory.
I want to change the processor in my code from a STM32G031K6T to a STM32G051K8T and I was careful to use only three timers that were in both chips. Everything else was compatible. UM1718 Chapter 15 told me how to do it. I have to keep it in the same directory for git.