Skip to main content
SG.4
Associate III
Jul 12, 2021 6:10 AM UTC
Solved

testing of ublox LARA R.211 a 4G LTE with stm32f745 controller using USB_Host middleware & USB_OTG_HS ?Can anybody help with the proper CubeMX parameters or are there any CDC USB host class examples so that this module detects a virtual com port.

If any examples on such please if anybody finds or could share some of their experience would be of great help.

Thanks in advance.

This topic has been closed for replies.
Walid ZRELLI
Walid ZRELLIBest answer
Visitor II
Jul 12, 2021 8:47 AM UTC

Hello @Community member​ ,

We provide some CDC USB host examples under our F7 Firmware Package.

Take a look at the example provided under the following path :

Firmware\Projects\STM32746G-Discovery\Applications\USB_Host\CDC_Standalone

You can be inspired by it.

BeST Regards,

Walid

3 replies

Walid ZRELLI
Walid ZRELLIBest answer
Visitor II
Jul 12, 2021 8:47 AM UTC

Hello @Community member​ ,

We provide some CDC USB host examples under our F7 Firmware Package.

Take a look at the example provided under the following path :

Firmware\Projects\STM32746G-Discovery\Applications\USB_Host\CDC_Standalone

You can be inspired by it.

BeST Regards,

Walid

SG.4
SG.4Author
Associate III
Jul 12, 2021 9:56 AM UTC

Hi @Walid ZRELLI​ ,

Thank you for the fastest response.

Its of great help indeed .

Thanks a lot again.

..

Hope you have a good day . Take Care.

Regards

--

Shweta

Walid ZRELLI
Visitor II
Jul 12, 2021 10:00 AM UTC

Glad to help you :smiling_face_with_smiling_eyes: You are welcome at any time.