Skip to main content
Associate
July 14, 2023
Solved

T = 1 Smartcard implementation with Cube MX

Hello ST electronics,

I wanted to know if there are any implementation of T= 1 protocol available with cube MX configurations.
Please do let me know.

Regards,
Adarsh T R

    This topic has been closed for replies.
    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    July 20, 2023

    There are many STM32s with smartcard interface that have a USART that supports the T=1 mode, e.g. STM32F0, STM32F3, STM32F7, STM32L4. The respective Reference Manual lists the available modes under the chapter USART extended features, e.g. Supports the T=0 and T=1 asynchronous protocols for smartcards as defined in the ISO/IEC 7816-3 standard.

    With CubeMX you can then select the smartcard mode for the respective supported USART, which essentially selects the bi-directional working pin and configures the smartcard function. There are indeed usually examples for T=0, but you can find information on the use of T=1 in the firmware X-CUBE-SMCARD, for example, and there specifically in the AN4800.

    Does it answer your question?

    Regards
    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    4 replies

    AdarshTRAuthor
    Associate
    July 14, 2023

    Smartcard ISO 7816

     

    Peter BENSCH
    ST Technical Moderator
    July 14, 2023

    If I understand you correctly, you want to manage the ISO 7816 smart card protocol in CubeMX, correct?

    Yes, this is possible if you have selected an STM32 that contains USARTs with this function. You only need to select one of the modes Smartcard or Smartcard with Card Clock for the USART in question.

    Regards
    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    AdarshTRAuthor
    Associate
    July 18, 2023

    Hello @Peter BENSCH,
    I have gone through the examples given for smartcard iso7816
    Smartcard_COMDMA
    Smartcard_T0
    Smartcard_T0_MFX
    The above are for T = 0 implementation. I wanted to know if there are any examples for T = 1 implementation.

    Regards,
    Adarsh TR

    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    July 20, 2023

    There are many STM32s with smartcard interface that have a USART that supports the T=1 mode, e.g. STM32F0, STM32F3, STM32F7, STM32L4. The respective Reference Manual lists the available modes under the chapter USART extended features, e.g. Supports the T=0 and T=1 asynchronous protocols for smartcards as defined in the ISO/IEC 7816-3 standard.

    With CubeMX you can then select the smartcard mode for the respective supported USART, which essentially selects the bi-directional working pin and configures the smartcard function. There are indeed usually examples for T=0, but you can find information on the use of T=1 in the firmware X-CUBE-SMCARD, for example, and there specifically in the AN4800.

    Does it answer your question?

    Regards
    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.