Skip to main content
Vegard Havellen
Associate II
Feb 21, 2017 10:10 PM UTC
Question

STMcubeMX don't generate code for DMA

Posted on February 21, 2017 at 23:10

Hi.

I am trying to generate code via STMcubeMX for UART via DMA. I have configured the UART and DMA correctly to my liking, but when I press generate source code the only code for the DMA is:

/**

* Enable DMA controller clock

*/

static void MX_DMA_Init(void)

{

/* DMA controller clock enable */

__HAL_RCC_DMA1_CLK_ENABLE();

}

When I look into the logfile for 

STMcubeMX I can see when it is trying to generate the code for the DMA it gives these errors:

[INFO] ImportTextPane:147 - (OptionalMessage_ERROR) IP (DMA) : Parameter (Channel) has Id (UART5_RX) currently not set

[INFO] ImportTextPane:147 - (OptionalMessage_ERROR) IP (DMA) : Parameter (PeriphDataAlignment) has Id (UART5_RX) currently not set

INFO] ImportTextPane:147 - (OptionalMessage_ERROR) IP (DMA) : Parameter (MemDataAlignment) has Id (UART5_RX) currently not set

[INFO] ImportTextPane:147 - (OptionalMessage_ERROR) IP (DMA) : Parameter (Mode) has Id (UART5_RX) currently not set

[INFO] ImportTextPane:147 - (OptionalMessage_ERROR) IP (DMA) : Parameter (FIFOMode) has Id (UART5_RX) currently not set

[INFO] ImportTextPane:147 - (OptionalMessage_ERROR) IP (DMA) : Parameter (FIFOThreshold) has Id (UART5_RX) currently not set

[INFO] ImportTextPane:147 - (OptionalMessage_ERROR) IP (DMA) : Parameter (FIFOThreshold) has invalid value (null)

[INFO] ImportTextPane:147 - (OptionalMessage_ERROR) IP (DMA) : Parameter (MemBurst) has Id (UART5_RX) currently not set

[INFO] ImportTextPane:147 - (OptionalMessage_ERROR) IP (DMA) : Parameter (MemBurst) has invalid value (null)

[INFO] ImportTextPane:147 - (OptionalMessage_ERROR) IP (DMA) : Parameter (PeriphBurst) has Id (UART5_RX) currently not set

[INFO] ImportTextPane:147 - (OptionalMessage_ERROR) IP (DMA) : Parameter (PeriphBurst) has invalid value (null)

When i look at the parameters it throws an error for I can see that it is set. 

Do anyone have a solution so I can generate code for the DMA?

Attached is the log-file and the IOC-file

#dma #stmcubemx #optionalmessage_error
This topic has been closed for replies.

6 replies

T J
Senior III
Feb 21, 2017 11:21 PM UTC
Posted on February 22, 2017 at 00:21

I have no trouble with CubeMX, for the DMA on Usarts... on the '091

are you using 1.7.0 ?

which processor is it ?

Vegard Havellen
Associate II
Feb 22, 2017 9:36 AM UTC
Posted on February 22, 2017 at 10:36

My STMcubeMX is on version 4.1.9, i am using STM32F446ZETx. 

ST Technical Moderator
Feb 22, 2017 10:34 AM UTC
Posted on February 22, 2017 at 11:34

Hello

‌,

Which version of HAL are you using ?

I created new project with your same configuration and I have

MX_DMA_Init() function as below

:

/** * Enable DMA controller clock */static void MX_DMA_Init(void){ /* DMA controller clock enable */ __HAL_RCC_DMA1_CLK_ENABLE();/* DMA interrupt init */ /* DMA1_Stream0_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA1_Stream0_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA1_Stream0_IRQn); /* DMA1_Stream1_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA1_Stream1_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA1_Stream1_IRQn);}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

Try creating new project in proper/new folder, thenkeep me informed about your updates.

Regards

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Vegard Havellen
Associate II
Feb 22, 2017 11:52 AM UTC
Posted on February 22, 2017 at 11:52

When I generated a new file I got the correct code and no errors in the log-file. Weird that it didn't work on my original project. I used version 1.6.0 of HAL. 

ST Technical Moderator
Feb 22, 2017 11:31 AM UTC
Posted on February 22, 2017 at 12:31

My STMcubeMX is on version 4.1.9

You should use the last version of STM32CubeMX 4.19.0

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Vegard Havellen
Associate II
Feb 22, 2017 12:33 PM UTC
Posted on February 22, 2017 at 12:33

Oh, sorry, I meant 4.19.0,