Skip to main content
JPard.2
Visitor II
Apr 27, 2021 9:12 AM UTC
Question

STMCubeIDE v1.6.1 silent failure generating peripheral files

When configuring TIM peripheral, result tim.c file has something that looks like a java runtime error dump (see attached file around line 110 and later): "FreeMarker template error (DEBUG mode; use RETHROW in production!):"

Steps to reproduce this:

  • Configure whatever peripheral you want( (tested on TIM and ADC).
  • Enable DMA and configure "DMA Request Synchronization Settings" to "Event Enable" with a request number 1 (but I think that the number doesn't matter).
  • Select save and generate project files. STMCubeIDE does the job without any error warnings but when open generated file you can see the problem.

Working in linux (Archlinux) without any problem until now.

Project configured for STM32H742ZITx.

Can somebody give a hint to solve this issue.

Thanks.

PD: It also happends with v1.6.0.

This topic has been closed for replies.