Skip to main content
perbaecklund9
Associate
Oct 20, 2014 9:39 AM UTC
Question

STM34CubeMX does not start

Posted on October 20, 2014 at 11:39

I had CubeMX installed and working fine. Then I updated the application and now all I see is dialog flashing by the says ''Check files''. After that nothing happens.

When I start it from a DOS box I get:

java -jar STM32CubeMX.exe

HeapMemory: 16252928

Using Application install path:C:\Program Files\STMicroelectronics\STM32Cube\STM

32CubeMX

Using Application install path:C:\Program Files\STMicroelectronics\STM32Cube\STM

32CubeMX

loadPluginJar : clock

loadPluginJar : add clock

loadPluginJar : filemanager

loadPluginJar : add filemanager

loadPluginJar : ipmanager

loadPluginJar : add ipmanager

loadPluginJar : pinoutconfig

InternalPropertyChange: ChangeKeepUser  dont care

loadPluginJar : add pinoutconfig

loadPluginJar : power

loadPluginJar : add power

loadPluginJar : projectmanager

This is Windows

This is 32 Bit VM

C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX\\db\plugins\projectman

ager\windows\32\toolgen.dll

loadPluginJar : add projectmanager

loadPluginJar : updater

Using Application install path:C:\Program Files\STMicroelectronics\STM32Cube\STM

32CubeMX

STM32CubeMX Software Update Start Now

I have reinstalled the program with the same result.

Suggestions?

#stmcube-stmcubemx-cube-stm32cube
This topic has been closed for replies.

9 replies

kolomaznik
Visitor II
Oct 20, 2014 10:06 AM UTC
Posted on October 20, 2014 at 12:06

I have the same problem.

yevgen
Associate
Oct 21, 2014 6:46 AM UTC
Posted on October 21, 2014 at 08:46

Hi !

I have the same problem on Windows7 & 8 64bits with clean and update installation of CubeMx.

What can be problem ?

DUrbano
Associate III
Oct 21, 2014 10:01 AM UTC
Posted on October 21, 2014 at 12:01

I have same problem and I don't understand why...

sdim
Associate II
Oct 22, 2014 1:28 PM UTC
Posted on October 22, 2014 at 15:28

I also have the same problem.

DUrbano
Associate III
Oct 22, 2014 3:10 PM UTC
Posted on October 22, 2014 at 17:10

I tried this: in my documents folder I found an .stm32cube folder and I deleted it. Re-installed last version of CubeMX and works fine (till now)

perbaecklund9
Associate
Oct 23, 2014 10:39 AM UTC
Posted on October 23, 2014 at 12:39

Thank you!

That helped.

kolomaznik
Visitor II
Oct 23, 2014 11:26 AM UTC
Posted on October 23, 2014 at 13:26

It helped

me

also

.

Thanks

stm32cube-t
ST Employee
Nov 19, 2014 2:33 PM UTC
Posted on November 19, 2014 at 15:33

Can you please indicate which version you started from and which version you upgraded to.

Thank you.

qwer.asdf
Senior
Nov 19, 2014 3:27 PM UTC
Posted on November 19, 2014 at 16:27

I had this problem when updating from 4.3 to 4.4. The update from 4.4 to 4.5 today was OK.