Skip to main content
Associate III
Oct 23, 2026 7:04 AM UTC
Question

STM32U083CCT6 HAL_StatusTypeDef Description Section

I am not sure but if this is a minor issue or should be fixed when working with STM32U083CCT6 MCU and those line is inside stm32u0xx_hal.c file.

Note: I can not add picture or drag it i dont know why.

 

* @brief Configure the Flash prefetch and the Instruction cache,

* the time base source, NVIC and any required global low level hardware

* by calling the HAL_MspInit() callback function to be optionally defined in user file

* stm32g0xx_hal_msp.c.

 

In the automatic generated comment lines it state that it was in stm32g0xx_hal_msp.c. If those kind of minor issues should be reported somewhere else , i use that place if i come accross the same situation again.(I am working with stm32u0xx by the way via CubeMX selection and code generation)

2 replies

mƎALLEm
ST Technical Moderator
Oct 23, 2026 8:24 AM UTC

Hello,

1- As the question is related to the HAL, it should be posted in STM32 MCUs Embedded software forum board. I’m moiving it then..

2- Please avoid asking more than one question in a thread. So for this question open a new thread and post it in STM32 MCUs Embedded software as it’s related to USBX:

By the way can i achive UX_Device_CDC_ACM_Standalone with my MCU? I am not sure if i can achieve this. In some LAB videos, they can achieve Standalone HID but i am not sure if it can be done for CDC_ACM standalone? I am struggling with CDC_ACM trying to do standalone without threadx, only usng usbx.

Thank you for your understanding.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Andrew Neil
Super User
Oct 23, 2026 8:44 AM UTC

 I can not add picture or drag it i dont know why

See:

 

Please also see:

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.