Skip to main content
Associate III
December 10, 2025
Solved

STM32N6 CubeMX I3C2 GPIO Configuration code missing from application context

  • December 10, 2025
  • 3 replies
  • 743 views

Hello,

With CubeMX version 6.16.0 and FW package version STM32Cube FW_N6 V1.3.0, the GPIO configuration's are missing from the generated HAL_I3C_MspInit and HAL_I3C_MspDeInit functions in stm32n6xx_hal_msp.c, when I3C is set to application context.

Application context stm32n6xx_hal_msp.c

/**
 * @brief I3C MSP Initialization
 * This function configures the hardware resources used in this example
 * @PAram hi3c: I3C handle pointer
 * @retval None
 */
void HAL_I3C_MspInit(I3C_HandleTypeDef* hi3c)
{
 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
 if(hi3c->Instance==I3C2)
 {
 /* USER CODE BEGIN I3C2_MspInit 0 */

 /* USER CODE END I3C2_MspInit 0 */

 /** Initializes the peripherals clock
 */
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_I3C2;
 PeriphClkInitStruct.I3c2ClockSelection = RCC_I3C2CLKSOURCE_CLKP;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /* Peripheral clock enable */
 __HAL_RCC_I3C2_CLK_ENABLE();
 /* USER CODE BEGIN I3C2_MspInit 1 */

 /* USER CODE END I3C2_MspInit 1 */

 }

}

 FSBL context stm32n6xx_hal_msp.c

/**
 * @brief I3C MSP Initialization
 * This function configures the hardware resources used in this example
 * @PAram hi3c: I3C handle pointer
 * @retval None
 */
void HAL_I3C_MspInit(I3C_HandleTypeDef* hi3c)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
 if(hi3c->Instance==I3C2)
 {
 /* USER CODE BEGIN I3C2_MspInit 0 */

 /* USER CODE END I3C2_MspInit 0 */

 /** Initializes the peripherals clock
 */
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_I3C2;
 PeriphClkInitStruct.I3c2ClockSelection = RCC_I3C2CLKSOURCE_CLKP;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /* Peripheral clock enable */
 __HAL_RCC_I3C2_CLK_ENABLE();

 __HAL_RCC_GPIOB_CLK_ENABLE();
 /**I3C2 GPIO Configuration
 PB11 ------> I3C2_SDA
 PB10 ------> I3C2_SCL
 */
 GPIO_InitStruct.Pin = CAM_I3C2_SDA_Pin|CAM_I3C2_SCL_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_PULLUP;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF2_I3C2;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 /* USER CODE BEGIN I3C2_MspInit 1 */

 /* USER CODE END I3C2_MspInit 1 */

 }

}

 

Best answer by Mahmoud Ben Romdhane

Hello @Tuomas95 

Issue is fixed in the latest STM32CubeMX release 6.17.0.

You can get it through this link.

Thanks

Mahmoud

 

3 replies

ST Technical Moderator
December 10, 2025

Hello @Tuomas95 

 

Let me thank you for posting.

For more investigation, I suggest that you provide your Ioc.File.

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ST Technical Moderator
December 11, 2025

Hello @Tuomas95 ,

 

Let me thank you for bringing this issue to our attention.

An internal ticket is submitted to the Dedicated Team (Internal Ticket Number: 223659)

I will let you know when the issue is fixed.

As Workaround, you can add the missing code lines manually.

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ST Technical Moderator
February 25, 2026

Hello @Tuomas95 

Issue is fixed in the latest STM32CubeMX release 6.17.0.

You can get it through this link.

Thanks

Mahmoud

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.