Skip to main content
reokyouma
Associate III
Mar 23, 2020 6:35 AM UTC
Question

STM32L4R9ZI, adding rtc wakeup standby mode to pre existing examples doesn't work

When I created a new project using the stm32cubeide, and set the new project to be able to go to standby mode and then wakeup using RTC timer, it works.

But when I try to add the standby mode with RTC Wakeup timer to a pre-existing example project, I can't seem to be able to wakeup from sleep but I am using the same configurations that I use in the new/blank project.

For Context, I am using the HAL Libraries to produce the standby mode and RTC Wakeup timer and adding it to the fp-ind-predmnt1 example project of ST, is there anything that I missed doing to configure the example project? also this example project doesn't have ioc so I don't know to configure anything that needs stm32cubemx ioc files

This topic has been closed for replies.

4 replies

Nesrine.JLASSI
Visitor II
Mar 23, 2020 10:05 AM UTC

Hello @reokyouma​ 

have you added the code for enabling the WakeUp ?

Regards,

Nesrine

reokyouma
reokyoumaAuthor
Associate III
Mar 23, 2020 10:28 AM UTC

am i right to assume this one ?

HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1);

I tried it but It didn't work out

uint8_t predrun =0;
int main(void)
{
 HAL_Init();
 
 HAL_PWREx_EnableVddIO2();
 __HAL_RCC_PWR_CLK_ENABLE();
 HAL_PWREx_EnableVddUSB();
 
 /* Configure the System clock */
 SystemClock_Config();
 
 
 RTC_init();
 
 if(__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET){
	 __HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);
	 __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
	 __HAL_RTC_ALARM_CLEAR_FLAG(&hrtc,RTC_FLAG_ALRAF);
 }
 predrun =0;
 InitTargetPlatform(TARGET_STWIN);
 
 t_stwin = HAL_GetTick();
 
 /* For enabling CRC clock for using motion libraries (for checking if STM32 microprocessor is used)*/
 MX_CRC_Init();
 
 /* Check the MetaDataManager */
 InitMetaDataManager((void *)&known_MetaData,MDM_DATA_TYPE_GMD,NULL); 
 
 PREDMNT1_PRINTF("\n\t(HAL %ld.%ld.%ld_%ld)\r\n"
 "\tCompiled %s %s"
 
#if defined (__IAR_SYSTEMS_ICC__)
 " (IAR)\r\n"
#elif defined (__CC_ARM)
 " (KEIL)\r\n"
#elif defined (__GNUC__)
 " (STM32CubeIDE)\r\n"
#endif
 "\tSend Every %4dmS Temperature/Humidity/Pressure\r\n"
 "\tSend Every %4dmS Acc/Gyro/Magneto\r\n"
 "\tSend Every %4dmS dB noise\r\n\n",
 HAL_GetHalVersion() >>24,
 (HAL_GetHalVersion() >>16)&0xFF,
 (HAL_GetHalVersion() >> 8)&0xFF,
 HAL_GetHalVersion() &0xFF,
 __DATE__,__TIME__,
 PERIOD_ENVIRONMENTAL,
 PERIOD_ACC_GYRO_MAG,
 MICS_DB_UPDATE_MUL_10MS * 10);
 
#ifdef PREDMNT1_DEBUG_CONNECTION
 PREDMNT1_PRINTF("Debug Connection Enabled\r\n");
#endif /* PREDMNT1_DEBUG_CONNECTION */
 
#ifdef PREDMNT1_DEBUG_NOTIFY_TRAMISSION
 PREDMNT1_PRINTF("Debug Notify Trasmission Enabled\r\n\n");
#endif /* PREDMNT1_DEBUG_NOTIFY_TRAMISSION */
 
 /* Set Node Name */
 ReCallNodeNameFromMemory();
 
 HCI_TL_SPI_Reset();
 
 /* Initialize the BlueNRG */
 Init_BlueNRG_Stack();
 
 /* Initialize the BlueNRG Custom services */
 Init_BlueNRG_Custom_Services(); 
 
 /* Check the BootLoader Compliance */
 PREDMNT1_PRINTF("\r\n");
 if(CheckBootLoaderCompliance()) {
 PREDMNT1_PRINTF("BootLoader Compliant with FOTA procedure\r\n\n");
 } else {
 PREDMNT1_PRINTF("ERROR: BootLoader NOT Compliant with FOTA procedure\r\n\n");
 }
 
 /* Set Accelerometer Full Scale to 2G */
 Set2GAccelerometerFullScale();
 
 /* initialize timers */
 InitTimers();
 
 /* Predictive Maintenance Initialization */
 InitPredictiveMaintenance();
 
 /* Infinite loop */
 while (1)
 {
 /* Led Blinking when there is not a client connected */
 if(!connected)
 {
 if(!TargetBoardFeatures.LedStatus) {
 if(!(HAL_GetTick()&0x3FF)) {
 LedOnTargetPlatform();
 }
 } else {
 if(!(HAL_GetTick()&0x3F)) {
 LedOffTargetPlatform();
 }
 }
 }
 
 if(set_connectable){ 
 if(NecessityToSaveMetaDataManager) {
 uint32_t Success = EraseMetaDataManager();
 if(Success) {
 SaveMetaDataManager();
 }
 }
 
 /* Now update the BLE advertize data and make the Board connectable */
 setConnectable();
 set_connectable = FALSE;
 }
 
 /* Handle user button */
 if(ButtonPressed) {
 ButtonCallback();
 ButtonPressed=0; 
 }
 
 if(PredictiveMaintenance){
 if (IsFirstTime)
 {
 IsFirstTime = 0;
 
	/* Initializes the MotionSP Vibration parameters */
 MotionSP_VibrationInit();
		
 if(FFT_Alarm)
 {
 /* Initialization of Alarm Status on Axes, Alarm Values Reported
 and Thresholds to detect WARNING and ALARM conditions */
 MotionSP_TimeDomainAlarmInit(&sTdAlarm, &sTimeDomainVal, &sTdRmsThresholds, &sTdPkThresholds);
 
 /* Frequency domain initialization of Alarm Status */
 MotionSP_FreqDomainAlarmInit(&FDWarnThresh, &FDAlarmThresh, &THR_Fft_Alarms, MotionSP_Parameters.subrange_num);
 }
 
 /* Configure the FIFO settings in according with others parammeters changed */
 MotionSP_ConfigFifo();
 
 enable_FIFO();
 
 /* Start of the Time Window */
 Start_Tick = HAL_GetTick();
 }
	 
 MotionSP_VibrationAnalysis();
 predrun=1;
 }
 
 /* handle BLE event */
 if(HCI_ProcessEvent) {
 HCI_ProcessEvent=0;
 hci_user_evt_proc();
 }
 
 /* Environmental Data */
 if(SendEnv) {
 SendEnv=0;
 SendEnvironmentalData();
 }
 
 /* Mic Data */
 if (SendAudioLevel) {
 SendAudioLevel = 0;
 SendAudioLevelData();
 }
 
 /* Motion Data */
 if(SendAccGyroMag) {
 SendAccGyroMag=0;
 SendMotionData();
 }
 
 /* Battery Info Data */
 if(SendBatteryInfo){
 SendBatteryInfo=0;
 SendBatteryInfoData();
 }
 if(!connected && predrun == 1){
 	predrun=0;
 	RTC_CalendarConfig();
 	HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1);
 	__HAL_RTC_ALARM_CLEAR_FLAG(&hrtc,RTC_FLAG_ALRAF);
 		 __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
 
 		 RTC_AlarmConfig();
// 	HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 0xFFFF, RTC_WAKEUPCLOCK_RTCCLK_DIV16);
 	HAL_PWR_EnterSTANDBYMode();
 }
 /* Wait for Event */
 //__WFI();
 }
}
 
 
void RTC_init(void){
	hrtc.Instance = RTC;
	hrtc.Init.HourFormat = RTC_HOURFORMAT_12;
	hrtc.Init.AsynchPrediv = 0x7F;
	hrtc.Init.SynchPrediv = 0xFF;
	hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
	hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
	hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
 
	if(HAL_RTC_Init(&hrtc) != HAL_OK){
		Error_Handler();
	}
 
}
void RTC_CalendarConfig(void){
	//this function does the rtc calendar config
 
	RTC_TimeTypeDef RTC_TimeInit;
	RTC_TimeInit.Hours = 12;
	RTC_TimeInit.Minutes = 11;
	RTC_TimeInit.Seconds = 0;
	RTC_TimeInit.TimeFormat = RTC_HOURFORMAT12_AM;
	HAL_RTC_SetTime(&hrtc, &RTC_TimeInit, RTC_FORMAT_BIN);
 
	RTC_DateTypeDef RTC_DateInit;
	RTC_DateInit.Date = 12;
	RTC_DateInit.Month = RTC_MONTH_JUNE;
	RTC_DateInit.Year = 18;
	RTC_DateInit.WeekDay = RTC_WEEKDAY_TUESDAY;
	HAL_RTC_SetDate(&hrtc, &RTC_DateInit, RTC_FORMAT_BIN);
 
 
 
}
 
void HAL_RTC_AlarmAEventCallback(RTC_HandleTypeDef *hrtc)
{
 
 /* Prevent unused argument(s) compilation warning */
// UNUSED(hrtc);
 
 /* NOTE : This function should not be modified, when the callback is needed,
 the HAL_RTC_AlarmAEventCallback could be implemented in the user file
 */
}
 
void RTC_AlarmConfig(void){
 
	RTC_AlarmTypeDef RTC_AlarmInit;
 
	memset(&RTC_AlarmInit,0,sizeof(RTC_AlarmInit));
 
	HAL_RTC_DeactivateAlarm(&hrtc, RTC_ALARM_A);
 
	RTC_AlarmInit.Alarm = RTC_ALARM_A;
	RTC_AlarmInit.AlarmTime.Hours = 12;
	RTC_AlarmInit.AlarmTime.Minutes = 11;
	RTC_AlarmInit.AlarmTime.Seconds=10;
 
	RTC_AlarmInit.AlarmTime.TimeFormat = RTC_HOURFORMAT12_AM;
	RTC_AlarmInit.AlarmMask = RTC_ALARMMASK_DATEWEEKDAY;
	RTC_AlarmInit.AlarmSubSecondMask = RTC_ALARMSUBSECONDMASK_NONE;
	if(HAL_RTC_SetAlarm(&hrtc, &RTC_AlarmInit, RTC_FORMAT_BIN) != HAL_OK){
		Error_Handler();
	}
}

should be the whole code

Nesrine.JLASSI
Visitor II
Mar 23, 2020 10:35 AM UTC

try this code,

/** Enable the WakeUp

*/

if (HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 0, RTC_WAKEUPCLOCK_RTCCLK_DIV16) != HAL_OK)

{

Error_Handler();

}

reokyouma
reokyoumaAuthor
Associate III
Mar 23, 2020 11:20 AM UTC

unfortunately it did't work

Correct me if I am wrong but aside from the code above, I need put this into the msp.c right?

void HAL_RTC_MspInit(RTC_HandleTypeDef* hrtc)
{
 //1. turn on LSE
 RCC_OscInitTypeDef RCC_OscInitStruct;
 
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSE;
 RCC_OscInitStruct.LSEState = RCC_LSE_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
 if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK){
	 Error_Handler();
 }
 
 //2 select LSE as RTC CLK
 RCC_PeriphCLKInitTypeDef RCC_RTCPeriphCLKInit;
 RCC_RTCPeriphCLKInit.PeriphClockSelection = RCC_PERIPHCLK_RTC;
 RCC_RTCPeriphCLKInit.RTCClockSelection = RCC_RTCCLKSOURCE_LSE;
 if(HAL_RCCEx_PeriphCLKConfig(&RCC_RTCPeriphCLKInit) != HAL_OK){
	 Error_Handler();
 }
 
 // 3 Enable the RTC Clock
 __HAL_RCC_RTC_ENABLE();
 
 //4 enable interrupt
 HAL_NVIC_SetPriority(RTC_Alarm_IRQn,15,0);
 HAL_NVIC_EnableIRQ(RTC_Alarm_IRQn);
 
}
 
/**
* @brief RTC MSP De-Initialization
* This function freeze the hardware resources used in this example
* @param hrtc: RTC handle pointer
* @retval None
*/
void HAL_RTC_MspDeInit(RTC_HandleTypeDef* hrtc)
{
 if(hrtc->Instance==RTC)
 {
 /* USER CODE BEGIN RTC_MspDeInit 0 */
 
 /* USER CODE END RTC_MspDeInit 0 */
 /* Peripheral clock disable */
 __HAL_RCC_RTC_DISABLE();
 /* USER CODE BEGIN RTC_MspDeInit 1 */
 
 /* USER CODE END RTC_MspDeInit 1 */
 }
 
}

and this one to the it.c

void RTC_Alarm_IRQHandler(void){
	HAL_RTC_AlarmIRQHandler(&hrtc);
}