Skip to main content
taz1000
Associate II
Jan 24, 2019 9:43 AM UTC
Question

STM32L412RBT6, CubeMX code for USB FS MSC doesn't work.

I have designed STM32L412RBT6 board with USB FS connection.

With CubeMX 5.0.0 and L4 firmware package V1.13.0, I generated USB MSC project for TrueStudio.

But, it doesn't work at all.

PC couldn't recognize my MCU.

For test, I changed the MCU to STM32F070RBT6 and generated USB MSC project with CubeMX.

Compiled with TrueSTUDIO.

It works OK.

Is there any known issue in my STM32L412RBT6 + CubeMX5.0 + L4_1.13.0 + TrueSTUDIO + USB FS MSC ?

* I need to confirm the HW is okay or not.

Is there any one who can upload any USB-ready firmware hex file for STM32L412RBT6 ?

Then, I can check my hardware with it.

This topic has been closed for replies.

8 replies

ST Technical Moderator
Jan 24, 2019 12:59 PM UTC

Hello,

Try to increase the heap and stack size (in Project Settings of CubeMX)

Kind Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
taz1000
taz1000Author
Associate II
Jan 25, 2019 9:01 AM UTC

Dear Imen,

I changed

Min. Heap Size -> 0x400

Min. Stack Size -> 0x800

But, the code doesn't work...

* I had compiled Nucleo-L412RB-P USB HID_Standalone project with Keil.

It works on my board.

It seems like that there is no problem in my HW.

Best Regards,

Danny

Tesla DeLorean
Guru
Jan 24, 2019 1:05 PM UTC

Do you have a crystal source on this board? What frequency?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
taz1000
taz1000Author
Associate II
Jan 25, 2019 9:02 AM UTC

Dear Clive,

I have 16MHz oscillator on board.

With RSS setting 'bypass', the tool did the clock configuration and there is no problem.

Best Regards,

Danny

MishaT
Associate II
Jan 28, 2019 10:54 AM UTC

Need increase Min. Heap Size and have 48Mhz clocks in USB. Min. Heap Size > MSC_MEDIA_PACKET.

taz1000
taz1000Author
Associate II
Jan 31, 2019 1:16 PM UTC

Dear MishaT,

I re-tried as your comment. But, it still fails.

Regards,

Danny

taraben
Associate III
Mar 25, 2019 5:49 PM UTC

Same Problem here.

I updated from CubeMX4 to CubeMX5 on my Board using STM32L486.

Now the same code does not work anymore.

It must be related with the Codegenerator or STM32L4 libs my strong impression is.

Unfortunately I can not simply go back in version with the codegenerator.

Anyone has an answer here?

Regards, Adib.

-

Manfred Dietrich
Associate II
Mar 25, 2019 9:51 PM UTC

Check the DP pullup:

USB_BCDR.DPPU

Regards Manfred