Skip to main content
Rob.Riggs
Senior
Oct 30, 2018 1:36 AM UTC
Question

STM32L4 HAL USB CDC: what does USBD_MAX_NUM_CONFIGURATION do?

STM32CubeMX and the L4 HAL 1.13.0 now sport an option to change the number of supported USB configurations.

I am trying to implement a USB interface that allows the host to choose between a CDC configuration that draws 500mA and one that draws 100mA. I have a battery powered device, and I want to present a CDC interface whether or not the battery can be charged.

It seemed like USBD_MAX_NUM_CONFIGURATION would help here. It seems to be a step in the right direction. I see two identical configurations enumerated. But I don't see any code in the USB layer that does anything with the configuration number when the host is enumerating or which would allow an application to alter or set a specific configuration.

Is there any documentation or example code illustrating how to make use of this new feature?

This topic has been closed for replies.