Skip to main content
WHuan.16
Associate
August 10, 2018
Question

STM32L100 watchdog setup

Hi Everyone,

I am using STM32L100RCT6 at the moment for my own personal project and I want to add watchdog function in my code especially IWDG. So I want to ask if there is any tutorial and example code I could use or does anyone has experience in setting it up. Sorry, I am a beginner and this is just the last bit of my own project. Many thanks

This topic has been closed for replies.

3 replies

ST Technical Moderator
August 10, 2018

Hello,

You can start from the IWDG example available within the STM32CubeL1 firmware package:

STM32Cube_FW_L1_V1.8.1\Projects\STM32L100C-Discovery\Examples\IWDG

So, you can check how this example was implemented and get inspiration to develop your application, it may helps you.

Have a look to your related reference manual in the section " Independent watchdog (IWDG)" and you can look on the attached presentation labs and follow "3.3.2 IWDG lab" section.

Hope this helps you.

With Regards,

Imen.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
WHuan.16
WHuan.16Author
Associate
August 13, 2018

@Imen DAHMEN​ ,

Hi, Imen.

There is nothing under Project file (not in version1.8.1 but 1.8.0 has the example) and I will definitely read the reference manual and the slides.

Thanks

WHuan.16
WHuan.16Author
Associate
August 13, 2018

@Imen DAHMEN​ 

Also, could I get slides for lab 0 as mentioned in the slides please?

I wonder if you would have slides for STM32L1 and slides to setup WWDG.

Kind Regardsm

William