Skip to main content
Associate II
March 22, 2026
Solved

STM32H7S3 CubeMX bug - ETH_CLK pin not initialized when using external clock source for Ethernet PHY

Hello,

I found a bug in STM32CubeMX code generation for STM32H7S3.

When configuring Ethernet with external clock input (ETH_CLK pin,
PD6 with AF4_ETH) as PHY clock source, CubeMX does not generate
GPIO initialization for this pin in HAL_ETH_MspInit().

Workaround - must add manually:

__HAL_RCC_GPIOD_CLK_ENABLE();
GPIO_InitStruct.Pin = GPIO_PIN_6;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF4_ETH;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

Without this, Ethernet does not work even though all other
ETH pins are correctly initialized by CubeMX.

Steps to reproduce:
1. Select STM32H7S3
2. Enable Ethernet (ETH)
3. Set clock source to external clock via ETH_CLK pin (PD6)
4. Generate code
5. ETH_CLK pin GPIO init is missing in generated code

CubeMX version: 6.17.0
MCU: STM32H7S3

Thank you

Ghofrane GSOURI
Ghofrane GSOURIBest answer
ST Technical Moderator
March 22, 2026

Hello @Happybolt 

Your contribution is much appreciated.

Issue has been escalated to dev team under internal ticket ID #0060894

I will keep you posted with updates.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

3 replies

TDK
March 22, 2026

Unable to duplicate. Please include your IOC file.

"If you feel a post has answered your question, please click ""Accept as Solution""."
HappyboltAuthor
Associate II
March 22, 2026

Made a new project and added ETH peripheral. PD6 (ETH_CLK) GPIO is not initialized in generated code. However, PHY clock generation is configured: PeriphClkInit.Eth1PhyClockSelection = RCC_ETH1PHYCLKSOURCE_HSE;

Ghofrane GSOURI
Ghofrane GSOURIBest answer
ST Technical Moderator
March 22, 2026

Hello @Happybolt 

Your contribution is much appreciated.

Issue has been escalated to dev team under internal ticket ID #0060894

I will keep you posted with updates.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.