Skip to main content
DTsai.1
Visitor II
Sep 27, 2021 11:05 AM UTC
Question

STM32H743ZIT lwip problem, STM32CubeMX v6, and STM32CUBE FW_H7 V1.8.0, MDK uVision v5.35, ARM Compiler v6, OS not used

Hello,

I make a Lwip project that was done on STM32CubeMX V6, and STM32CUBE FW_H7 V1.8.0. This project can't work when build with MDK uVision v5.35, ARM Compiler v6. When pinging the device, there is no response!

But it can work well after changed the Compiler to "ARM Compiler v5".

Please help as this is really confusing.

Thank you in advance for your help.

This topic has been closed for replies.

1 reply

alister
Senior III
Sep 27, 2021 10:13 PM UTC

You have to learn it. Read its docs. Break your project down into smaller parts. E.g. start with LED flash.