Associate
Nov 2, 2021 10:26 AM UTC
Question
STM32H743ZI SPI Clock enhancement options
- 6 replies
- 1409 views
Hi ST Support,
I have an STM32H743ZI and use SPI4 for the SPI communication.
I have generated the Project from the Cube MX and configured an SPI clock of 50Mhz, But on the Logic analyzer captures, I can see only the clock of 25Mhz. We are trying to interface with some Slaves where STM32H743ZI is a DMA Master.
It would be great if we get some code that can show us a Clock frequency of 50Mhz on the Logic analyzer.
I am attaching the Cube MX file for reference.