Skip to main content
Associate II
February 23, 2024
Solved

STM32H725ZGT6 custom board hangs (Cube, Keil, ULINK2)

Hello,

 

i am using the STM32H725ZGT6 on a custom layout.

As comparison i am also using the STM32H723ZGT6U on a NUCLEO-H723ZG Board.

I am using STM32CubeMX, Keil µVision and the ULINK2 debugger. 

 

To test the Serial Wire Flashing procedure, i created an empty Cube Projext (using HSI and no controller pins), compiled itand flashed it to the controller. The Nucleo Board works perfectly fine with this setup.

 

However when i do the exact same procedure (of corse with correct controller), my custom Board has a problem:

I can only flash the software when the BOOT0-Pin is set to +3V3 (but not use any peripherals). When the BOOT0-pin is set to GND, i cannot program anymore and there is "SWD Communication Failure" according to Keil. I also tried to toggle a GPIO but had no acces with my custom board so far.

Any ideas on this?

If you need more infos, please let me know.

See Layout files attached. Thanks.

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
February 23, 2024

Check LDO vs SMPS settings in your System Clock Configuration code.

Check VOS and PLL settings.

Check HSE_VALUE 

 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

4 replies

ST Technical Moderator
February 23, 2024

Hello @TimK1 

Is GND connected to the debugger? Try powering the board directly from the debugger.

Check the debugger settings to set correct debugger and use SWD.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
TimK1Author
Associate II
February 23, 2024

Hello Imen,

thank you for the reply. Yes, i have connected GND and VCC to my custom board. However i think the ULINK2 is not able to power the board. It has a jumper +3V3 / VCC / ARM. But this only powers the SWD signals, not the VCC of the board (as far as i can see). I tried both jumper positions with no change of the outcome. 

Greets, Tim

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
February 23, 2024

Check LDO vs SMPS settings in your System Clock Configuration code.

Check VOS and PLL settings.

Check HSE_VALUE 

 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
TimK1Author
Associate II
February 23, 2024

Hello Tesla,

thanks for your reply. This solved my problem. 

In STM Cube i had the wrong setting. (SMPS instead of LDO):

System Core -> RCC -> Parameter Settings -> Power Parameters -> PWR_LDO_SUPPLY

Thank you very much!