Skip to main content
Explorer II
April 18, 2025
Solved

STM32H7232ZG CORDIC DMA code generation issue

I would like to file a bug report for STM32CubeMX.

During configuration of CORDIC using DMA, I have found the following issue:

In:

void HAL_CORDIC_MspInit(CORDIC_HandleTypeDef* hcordic)
{
 if(hcordic->Instance==CORDIC)
 {
 /* USER CODE BEGIN CORDIC_MspInit 0 */

 /* USER CODE END CORDIC_MspInit 0 */
 /* Peripheral clock enable */
 __HAL_RCC_CORDIC_CLK_ENABLE();

 /* CORDIC DMA Init */
 /* CORDIC_WR Init */
 hdma_cordic_wr.Instance = DMA1_Stream0;
 hdma_cordic_wr.Init.Request = DMA_REQUEST_CORDIC_WRITE;
 hdma_cordic_wr.Init.Direction = DMA_MEMORY_TO_PERIPH;
 hdma_cordic_wr.Init.PeriphInc = DMA_PINC_DISABLE;
 hdma_cordic_wr.Init.MemInc = DMA_MINC_ENABLE;
 hdma_cordic_wr.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;
 hdma_cordic_wr.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;
 hdma_cordic_wr.Init.Mode = DMA_NORMAL;
 hdma_cordic_wr.Init.Priority = DMA_PRIORITY_LOW;
 hdma_cordic_wr.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
 if (HAL_DMA_Init(&hdma_cordic_wr) != HAL_OK)
 {
 Error_Handler();
 }

 __HAL_LINKDMA(hcordic,hdmaOut,hdma_cordic_wr);

 /* CORDIC_RD Init */
 hdma_cordic_rd.Instance = DMA1_Stream1;
 hdma_cordic_rd.Init.Request = DMA_REQUEST_CORDIC_READ;
 hdma_cordic_rd.Init.Direction = DMA_PERIPH_TO_MEMORY;
 hdma_cordic_rd.Init.PeriphInc = DMA_PINC_DISABLE;
 hdma_cordic_rd.Init.MemInc = DMA_MINC_ENABLE;
 hdma_cordic_rd.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;
 hdma_cordic_rd.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;
 hdma_cordic_rd.Init.Mode = DMA_NORMAL;
 hdma_cordic_rd.Init.Priority = DMA_PRIORITY_LOW;
 hdma_cordic_rd.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
 if (HAL_DMA_Init(&hdma_cordic_rd) != HAL_OK)
 {
 Error_Handler();
 }

 __HAL_LINKDMA(hcordic,hdmaIn,hdma_cordic_rd);

 /* USER CODE BEGIN CORDIC_MspInit 1 */

 /* USER CODE END CORDIC_MspInit 1 */

 }

}

The DMA streams are linked to the wrong DMA handles, I had to manually adjust the following to get the CORDIC working with DMA:

__HAL_LINKDMA(hcordic,hdmaOut,hdma_cordic_wr); -> __HAL_LINKDMA(hcordic,hdmaIn,hdma_cordic_wr);

and:

__HAL_LINKDMA(hcordic,hdmaIn,hdma_cordic_rd); -> __HAL_LINKDMA(hcordic,hdmaOut,hdma_cordic_rd);

 

This issue happens when generating code using STM32CubeMX version 6.14.0. The issue can be reproduced by simply creating a project for the NUCLEO-H723ZG, initializing the CORDIC with the write and read DMA streams enabled and then generating the code. 

 

Note: The CORDIC_Sin_DMA example shows the correct HAL_CORDIC_MspInit function. This example was used to pinpoint why the CORDIC wasn't working in a newly created project.

This topic has been closed for replies.
ST Technical Moderator
April 18, 2025

Hello @beauwilmink ,

 

Thank you for binging this issue to our attention.

An internal ticket is raised to the Development team under this number: 208115.

 

Thanks.

Mahmoud

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

ST Technical Moderator
April 18, 2025

Hello @beauwilmink ,

 

First let me thank you for posting and welcome to the ST Community.

Your request is under investigation, and I will get back to you ASAP.

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ST Technical Moderator
April 18, 2025

Hello @beauwilmink ,

 

Thank you for binging this issue to our attention.

An internal ticket is raised to the Development team under this number: 208115.

 

Thanks.

Mahmoud

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.