Skip to main content
MMedv
Associate II
June 1, 2021
Question

STM32H7 dual core support

  • June 1, 2021
  • 6 replies
  • 2314 views

Does ST publish a roadmap of features/enhancements for CubeIDE? I'd really like to know what is planned for STM32CubeIDE for the dual core H7 chips.

For example, in Project Manager->Project, there is a setting "Dual Core Boot Mode", but it is greyed out. When will this be available? I'd like my CM4 to do boot initialization (for example of the RCC) rather than the CM7, but it seems this is not possible to generate out of CubeIDE right now.

This topic has been closed for replies.

6 replies

Markus GIRDLAND
ST Employee
June 1, 2021

Hello!

We don't have a public roadmap of planned features that we publish anywhere. This specific feature is currently not on the roadmap.

MMedv
MMedvAuthor
Associate II
June 1, 2021

@Markus GIRDLAND​ So essentially, if you plan on using an H7 dual core chip, you can't count on using CubeIDE/MX at all. Only in the very narrow way ST currently has it set up. That is a bummer because CubeIDE/MX is so helpful in getting your HW setup correct. That's almost enough to discourage me from using the chip in a new design.

Associate
December 27, 2024

And 3.58 years later, "Dual Core Boot Mode" is still greyed out .... :(

Associate III
December 30, 2024

They've probably got the whole dev team working on hype-y AI features like all tech companies right now. Sigh.

Associate
December 30, 2024

Agreed.

Haven't we all learned the lessons from "hype-space cyberspace" ?