Skip to main content
MzMCeotronicsAG
Visitor II
Sep 22, 2021 10:18 AM UTC
Solved

Stm32H7, CubeMX, CMSIS V2, FreeRTOS: Interrupts disabled while creating new task, but not enabled again until scheduler is started.

When creating a new Freertos Task like this:

osThreadNew(StartDefaultTask, NULL, &defaultTask_attributes);
prvAddNewTaskToReadyList(...)

will be called and uses

taskENTER_CRITICAL()

to disable interrupts. This breaks down to the call of void vPortEnterCritical( void )

void vPortEnterCritical( void )

which increases uxCriticalNesting by one.

Before leaving

void vPortExitCritical()

is called. This function should decrease uxCriticalNesting and reactivate interrupts if uxCriticalNesting == 0.

However, uxCriticalNesting was previously initialized with  0xaaaaaaaa. So that uxCriticalNesting == 0 is not reached.

A later call of

osKernelStart();

finally sets uxCriticalNesting to 0 and reactivates all interrupts.

This results in deactivated interrupts between the first task creation and kernel start, which has undesirable side effects such as the systick timer being stopped, which results in a broken HAL_Delay() function.

This topic has been closed for replies.
Walid ZRELLI
Walid ZRELLIBest answer
Visitor II
Sep 30, 2021 9:55 AM UTC

Hello @Mathieu Münch-zur Megede​ ,

This is intentional from the FreeRTOS maintainer. Please see this comment.

BeST Regards,

Walid

4 replies

Walid ZRELLI
Visitor II
Sep 30, 2021 8:34 AM UTC

Hello @Mathieu Münch-zur Megede​ 

This issue has been internally raised. I will keep you posted.

Thanks for your contribution.

BeST Regards,

Walid

Walid ZRELLI
Visitor II
Sep 30, 2021 8:35 AM UTC

Internal ticket number: 114615 (PS: This is an internal tracking number and is not accessible or usable by customers)

Walid ZRELLI
Walid ZRELLIBest answer
Visitor II
Sep 30, 2021 9:55 AM UTC

Hello @Mathieu Münch-zur Megede​ ,

This is intentional from the FreeRTOS maintainer. Please see this comment.

BeST Regards,

Walid

Pavel A.
Sep 30, 2021 2:40 PM UTC

> systick timer being stopped, which results in a broken HAL_Delay() function.

Let's see. vPortEnterCritical executes vPortRaiseBASEPRI which is raises basepri to configMAX_SYSCALL_INTERRUPT_PRIORITY.

So, interrupts of priority greater than configMAX_SYSCALL_INTERRUPT_PRIORITY will work before the scheduler starts.

These interrupts cannot call FreeRTOS functions anyway.

Just use a different timer for the HAL tick, as recommended by CubeMX/CubeIDE. Set it's priority high.