Skip to main content
Associate III
January 16, 2026
Question

[STM32H563ZIT Dev Board] Error when generating SDMMC files using CMake - STMCubeMX version 6.16.1

Hello!

I tried to generate the code for SDMMC using CMake, but was facing an error that did not let me finish building the project. The error was:
".../FileX/Target/fx_stm32_sd_driver_glue.c:40:(.text.fx_stm32_sd_init+0xc): undefined reference to `MX_SDMMC1_SD_Init'".

Also, using ThreadX and FileX. In FileX I enabled the setting "FX Driver Initializes the SD IP" (set to true).

I saw that the MX_SDMMC1_SD_Init function is inside the main.c file, but it is declared with the "static". So, right now, to be able to build the project with CMake, I need to manually remove the "static" from the MX_SDMMC1_SD_Init function definition in main.c file.

2 replies

ST Technical Moderator
January 16, 2026

Hello @Sander_UP 

Thanks for reporting this in STCommunity,

I'm currently investigating internally this behavior. I will get back to you asap.

KR, Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
ST Technical Moderator
January 16, 2026

Hello @Sander_UP 

After checking, it seems that the issue only occurs when enabling the setting 'FX Driver Initializes the SD IP' under SD Driver. This issue has been raised internally to the dedicated team for further investigation. 

 (Ticket 225325 This is an internal tracking number and is not accessible or usable by customers.)

Thanks,

KR, Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.