Skip to main content
char_array
Associate III
Jan 5, 2022 4:29 PM UTC
Solved

STM32G4 RX DMA not working

I tested the sending with a USB-serial converter and I can see the MCU is sending. Looping back the TX signal to the RX on the board doesn't result in receiving data, nor does connecting the TX of the USB-serial converter. However I do get RX line error interrupts if I connect the wire, and if I enable idle line interrupt that works too.

Here is my stripped down code:

#include "app_main.h"
 
#include "main.h" // includes correct STM32 HAL
 
//RTOS includes
#include "FreeRTOS.h"
#include "task.h"
#include "cmsis_os2.h"
 
#include <stdio.h>
#include <sys/unistd.h>
 
#ifdef DEBUG
 
extern "C" int _write(int file, char* data, int size)
{
 if ((file != STDOUT_FILENO) && (file != STDERR_FILENO))
 {
 return -1;
 }
 
 for(int i = 0; i < size; ++i)
 {
 ITM_SendChar(data[i]);
 }
 
 return size;
}
#endif
 
static TaskHandle_t appMainTaskHandle;
static constexpr UBaseType_t APP_MAIN_TASK_PRIORITY = ( UBaseType_t ) (osPriorityNormal) ;
static constexpr size_t APP_MAIN_TASK_STACK_SIZE_BYTES = 2048;
 
extern UART_HandleTypeDef huart1;
 
/*
USART1:
PC4 TX
PC5 RX
*/
 
static void uartTestTask(void* arg)
{
 constexpr size_t m_BUFFER_SIZE = 50;
 uint8_t m_rxBuffer[m_BUFFER_SIZE];
 
 const uint8_t* m_rxTail;
 
 UART_HandleTypeDef* const m_pUartHandle = &huart1;
 
 m_rxTail = m_rxBuffer; // reset buffer
 HAL_UART_Receive_DMA(m_pUartHandle, (uint8_t*)m_rxBuffer, m_BUFFER_SIZE); // start DMA reception
 
 while(1)
 {
 
 size_t len;
 
 const uint8_t* rxHead = m_rxBuffer + m_BUFFER_SIZE - m_pUartHandle->hdmarx->Instance->CNDTR;
 
 if (rxHead >= m_rxTail)
 {
 len = rxHead - m_rxTail;
 }
 else
 {
 len = rxHead - m_rxTail + m_BUFFER_SIZE;
 }
 
 printf("len: %d\n", len);
 
 HAL_UART_Transmit(m_pUartHandle, (uint8_t*)"test\n", 5, 1000);
 
 vTaskDelay(1000 / portTICK_PERIOD_MS); //startup delay
 }
}
 
 
static void appMainTask(void* arg)
{
 vTaskDelay(10 / portTICK_PERIOD_MS); //startup delay
 
 [[maybe_unused]] BaseType_t res = 
 xTaskCreate(
 uartTestTask,
 "uartTestTask",
 APP_MAIN_TASK_STACK_SIZE_BYTES/4,
 NULL,
 APP_MAIN_TASK_PRIORITY,
 NULL );
 
 
 while(1)
 {
 vTaskDelay(1000 / portTICK_PERIOD_MS);
 }
}
 
extern "C" bool startAppMainTask()
{
 BaseType_t res = xTaskCreate( appMainTask,
 "appMain",
 APP_MAIN_TASK_STACK_SIZE_BYTES/4,
 NULL,
 APP_MAIN_TASK_PRIORITY,
 &appMainTaskHandle );
 return res == pdPASS;
}

This topic has been closed for replies.
TDK
TDKBest answer
Jan 5, 2022 4:41 PM UTC

https://community.st.com/s/question/0D53W00001EzCmCSAV/mxdmainit-order-in-the-mainc-file-generated-by-stm32cubemx-how-to-fix

"If you feel a post has answered your question, please click ""Accept as Solution""."

2 replies

char_array
Associate III
Jan 5, 2022 4:35 PM UTC

I found the answer. STM32CubeMX initialized the DMA after the UART. It needs to be initialized before the UART.

I will check if a newer version of CubeMX fixed the bug.

TDK
TDKBest answer
Jan 5, 2022 4:41 PM UTC
"If you feel a post has answered your question, please click ""Accept as Solution""."