Skip to main content
MKanc.1
Associate III
Jan 27, 2025 2:54 AM UTC
Solved

STM32G030F6P ADC Frequency in STM32CubeMX

I was checking maximum frequencies of some MCUs and noticed i can pick ADC frequency in CubeMX clock configuration up to 80MHz for TSSOP-20 STM32G030. Its maximum frequency is 64MHz.

Datasheet states it can deliver maximum 2Msps on 12 bit but with its 1.5 Sampling and 12.5 conversion cycles it reaches way higher sample rates.

I checked some of the reference manual chapters and did not noticed anything unusual, prescalers seems to accept /1 divisions as well.

I am not familiar with reference manuals. Datasheet 5.3.17 also shows 35MHz maximum frequency. What's the thing i am missing? Is it a bug on interface?

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Jul 10, 2025 8:19 AM UTC

Hello @MKanc.1 

This issue is fixed in the latest release of CubeMX v6.15.0.

Thank you for your contributions.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

5 replies

ST Technical Moderator
Jan 27, 2025 1:36 PM UTC

Hello @MKanc.1 ,

The maximum frequency of STM32G030 is 64MHz as mentioned in the Datasheet.

Which CubeMX version used?

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
MKanc.1
MKanc.1Author
Associate III
Jan 27, 2025 1:43 PM UTC

I had 6.12.x something before, updated to 6.13.0 and it is still same.

Stm32CubeIDE 1.16.1 have same issue, accepting ADC frequency up to 80 MHz.

ST Technical Moderator
Jan 27, 2025 3:34 PM UTC

Hi @MKanc.1 ,

An internal ticket (ID 201535) is submitted to fix this.

Thank you for your contribution and for bringing this issue to our attention.

(PS: internal ticket ID 201535 is an internal tracking number and is not accessible or usable by customers).

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Imen.DBest answer
ST Technical Moderator
Jul 10, 2025 8:19 AM UTC

Hello @MKanc.1 

This issue is fixed in the latest release of CubeMX v6.15.0.

Thank you for your contributions.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Ozone
Principal
Jul 10, 2025 9:03 AM UTC

> ...CubeMX clock configuration up to 80MHz for TSSOP-20 STM32G030. Its maximum frequency is 64MHz.

> I am not familiar with reference manuals. Datasheet 5.3.17 also shows 35MHz maximum frequency. What's the thing i am missing? Is it a bug on interface?

Those are the maximal clock frequencies for the ADC peripheral units, not sampling rates. You probably noticed.

> I checked some of the reference manual chapters ...

I would highly suggest to read the full ADC section of the reference manual, it describes this unit in detail - including all the sequential steps involved until you get the ADC output.

Other STM32 devices have several ADC units that can work in interleaved mode, and thus doubling or tripling the effective sampling rate.
However, designing proper analogue hardware to support such high sampling rates with acceptable accuracy is far from trivial either.