Skip to main content
EBAHI.1
Associate II
Dec 20, 2022 9:58 AM UTC
Question

STM32F7xx Eth with CubeIDE Update 1.11.0

I have wrote an product with tcp communication, last modification September 2021...

Today I need a small evolution ( move from HSI-RC to HSE)...the Ethernet does not run now.

I have try to work with doc concerning the new driver versus legacy...

help-me.

Eric

This topic has been closed for replies.

3 replies

Pavel A.
Dec 20, 2022 10:51 AM UTC

Does it work with the new driver before changing the clock source from HSI to HSE?

EBAHI.1
EBAHI.1Author
Associate II
Dec 20, 2022 11:00 AM UTC

All the application is running (FreeRTos, CAN, USARTs, timer, GPIO) but it does not send TCP packet.

I try to DO NOT change my code... just config 8742 in CubeMx...

I use tcp_send, tcp_write,tcp_sndbuf, tcp_output, tcp_abort, tcp_close......

EBAHI.1
EBAHI.1Author
Associate II
Dec 20, 2022 11:06 AM UTC

Today I work back on the old hardware with HSI-rc to try to minimize the problemssss