Skip to main content
MOlma.1
Associate
Jan 20, 2020 6:06 PM UTC
Question

stm32f7-discovery board. The board is missing from selection of STM32CubeIDE (Ver 1.2.0).

On the same computer it is present in the selection list of STM32CubeMX 5.5.0 . Answers on internet not found. I need it in IDE.

OS is Win 7 Professional SP1 . MCU STM32F746NGH6.

I have downloaded stm32cube_fw_f7_v150.zip, stm32cube_fw_f7_v151.zip and stm32cube_fw_f7_v1150.zip in repository .

This topic has been closed for replies.

6 replies

Cartu38 OpenDev
Graduate II
Jan 20, 2020 9:34 PM UTC

According to me board STM32746G-EVAL is the one you're looking for (STM32F746NGHx soldered on). Such board is highlited as NRND (Not Recommended for New Design means obsolete soon) but still supported. I'm STM32CubeIDE 1.2.0 based.

MOlma.1
MOlma.1Author
Associate
Jan 20, 2020 10:38 PM UTC

Is there a known way to force STM32CubeIDE 1.2.0 to enable designs based on "Not Recommended for New Design" boards?

At customers own risk, of course.

Cartu38 OpenDev
Graduate II
Jan 21, 2020 6:17 AM UTC

Still according what i'm able to do as STM32CubeIDE end user​ NRND is allowing to work with this target. Just sharing such may phase out in some near future.

MOlma.1
MOlma.1Author
Associate
Jan 21, 2020 6:00 PM UTC

Is there a way to make it appear in the list if it is not there?

cqexbesd
Associate
Feb 15, 2020 9:42 PM UTC

1.2.0 is also missing NUCLEO-F439ZI which is still "Active" so I think the NRND isn't the cause of the OPs board being missing. A related question would be - are there any resources explaining how to add new boards to the IDE? Any place where one could download pre-done definitions from? Any charts showing boards that are roughly equivalent for IDE purposes?

cqexbesd
Associate
Feb 16, 2020 9:09 PM UTC

This doesn't help the OP but for people finding this in a search - it looks like you can use NUCLEO-F429ZI as a substitute for NUCLEO-F439ZI as the only difference I can see is the addition of hardware accelerated crypto.