Skip to main content
THosh
Associate
Sep 7, 2018 1:22 AM UTC
Question

[STM32F429I-DISC1]USB not responsed

HI, There .

​

I bought STM32F429I-DISC1 evaluation board.

In first. I download demonstration firmware.

\STM32Cube_FW_F4_V1.21.0\Projects\STM32F429I-Discovery\Demonstrations\STemWin

​

Run that . feel so good .ST-LINK is active and I can see USB Mass storage.

but not responsed when USB USER connected(CN6).

and freeze when I chooose FileViewer in top nemu.

​

I think 1more mass storage confirm when USB USER connect.Is it misunderstand?

​

I checked device manager in windows.it is host of USB.

unknown device was detected.Need I get driver for that device??

​

Pls help me. How to resolve it or where check ?

​

Thanks in advance.

This topic has been closed for replies.

2 replies

THosh
THoshAuthor
Associate
Sep 7, 2018 1:46 AM UTC

device id of unknown device

USB\VID_0483&PID_374B&REV_0100&MI_02

Pavel A.
Sep 7, 2018 9:37 PM UTC

Device USB\VID_0483&PID_374B&REV_0100 is the STLink debugger.

The driver for it is available on ST.com.

It has several variants, your variant seems to be a multifunction device and the other function is likely a "virtual COM port".

-- pa