Skip to main content
MHama.3
Associate II
Mar 25, 2022 7:23 AM UTC
Question

stm32f407 Lwip without FreeRtos

Hello community

I am working with the stm32f407 on a Project with Lwip without FreeRtos. The code worked on version 1.7.0. but when i changed to 1.9.0 I got hardfault, I solved the problem by putting the LWIP_RAM_HEAP_POINTER on address 0x2001C000(SRAM2). but I still can't ping the board. 

The LWIP_RAM_HEAP_POINTER on 1.7.0 could not be set at all in the MX configuration.

Does anyone have any idea.

many greetings

Mosaab

This topic has been closed for replies.

6 replies

EErik.1
Visitor II
Mar 27, 2022 10:03 PM UTC

Hello MHama.3,

I have same problem. Did you solve the pinging problem?

MHama.3
MHama.3Author
Associate II
Mar 28, 2022 5:57 AM UTC

Hello EErik. 1,

unfortunately not yet.

EErik.1
Visitor II
Mar 29, 2022 7:17 PM UTC

Hello MHama.3,

I solved the pinging problem.

I disabled CHECKSUM_CHECK_ICMP and CHECKSUM_GEN_ICMP in the Cube Mx LWIP configiration checksum tab. Then pinging is ok.

MHama.3
MHama.3Author
Associate II
Mar 31, 2022 7:55 AM UTC

I have already done the same but still can't pingging

Aziz BRIGUI
ST Technical Moderator
Mar 30, 2022 8:40 AM UTC

Hello @MHama.3​ ,

Thank you for your feedback.

Please refer to this thread :

F4 + FreeRTOS + LwIP. Bad default LWIP_RAM_HEAP_POINTER after updating to v1.9.0. (st.com)

If your issue is solved, please close this post by clicking the "Select as Best" button. This will help other members of the community find this response more quickly.

Best regards,

Aziz

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.