Skip to main content
DA.1115
Associate
May 26, 2020 1:47 PM UTC
Question

STM32F205VGTx - Need support to enable the USB OTG High speed Dual role using the STM32CubeMx V5.6.1

Hi all, Thanks for the support. I am using STM32CubeMx V5.6.1 to generate the driver for STM32F205VGTx USB OTG High speed dual role function.

I required USB OTG High speed for communication between to STM32 controller. So I am trying to enable using the STM32CubeMx V5.6.1. But I see WARNING as "This IP has no parameter to be configured"(Refer Image attached).

  1. Why the WARNING is shown?
  2. What is the impact due to this WARNING?

Thanks for sharing the experience.

This topic has been closed for replies.

1 reply

MBugl.2
Visitor II
Nov 23, 2020 7:57 AM UTC

This should not be a problem.

The real problem is the Middleware USB_HOST and USM_DEVICE disabled.

Reading other old questions (2015 https://community.st.com/s/question/0D50X00009XkgMdSAJ/mx-usb-and-host-vs-device-support) I think the only solution is a DIY approach.

During last 5 years no improvements from ST on this?

(I asked my FAE but I got no answer)