Skip to main content
David Martins
Senior
May 10, 2018 2:32 PM UTC
Question

STM32f070F6 with CDC HAL libs?

Posted on May 10, 2018 at 16:32

Hi.

I'm trying to upgrade an existing PCB (so changing the MCU is not an option for now).

The MCU used so far is the STM32f070F6. The MCU has USB peripheral and I want to use this as VCOM.

When I generate the code with CubeMX and try to compile (with absolutely no code change), I get the message that the MCU do not have enough RAM: '/arm-none-eabi/bin/ld.exe: region` RAM 'overflowed by 1760 bytes'.

I have already changed the CDC buffers to a size of 40 bytes (maximum of what I want to transfer), but I still have a similar error.

Is there an example with this MCU in which the USB peripheral is used?

Thank you.

#cubemx #usbvcom #stm32f070f6 #stm32f070
This topic has been closed for replies.

15 replies

Khouloud GARSI
ST Employee
May 10, 2018 3:54 PM UTC
Posted on May 10, 2018 at 17:54

Hi David,

There is an application under the

http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-mcu-packages/stm32cubef0.html

package. It's titled 'CDC_Standalone' and could be found following the path below:

STM32Cube_FW_F0_V1.9.0\Projects\STM32072B_EVAL\Applications\USB_Device\CDC_Standalone

The example may help you to correctly configure your application. It shows how to use the STM32F0xx USB Device peripheral where the STM32 MCU behaves as a USB-to-RS232 bridge following the Virtual COM Port (VCP) implementation. 

Khouloud.

David Martins
Senior
May 11, 2018 4:52 PM UTC
Posted on May 11, 2018 at 16:52

Thank you

garsi.khouloud

I'm following this example, but the problem is that I can not compile at all.

I still have RAM overflow.

The project is here (

https://mega.nz/#F!ke5S0JoJ!tJqNLGDPO_OMfP3whwUPrg

).

As you can see, there is no modified code. It's a clean project, but apparently there is not enough RAM ...

arm-none-eabi-gcc -mcpu=cortex-m0 -mthumb -mfloat-abi=soft -specs=nosys.specs -specs=nano.specs -T'../STM32F070F6Px_FLASH.ld' -Wl,-Map=output.map -Wl,--gc-sections -o 'stm_vcom.elf' @'objects.list' -lm

c:/ac6/systemworkbench/plugins/fr.ac6.mcu.externaltools.arm-none.win32_1.0.201708311556/tools/compiler/bin/../lib/gcc/arm-none-eabi/6.3.1/../../../../arm-none-eabi/bin/ld.exe: stm_vcom.elf section`.bss' will not fit in region `RAM'

c:/ac6/systemworkbench/plugins/fr.ac6.mcu.externaltools.arm-none.win32_1.0.201708311556/tools/compiler/bin/../lib/gcc/arm-none-eabi/6.3.1/../../../../arm-none-eabi/bin/ld.exe:region `RAM' overflowed by 1632 bytes

collect2.exe: error: ld returned 1 exit status

make: *** [stm_vcom.elf] Error 1

makefile:37: recipe for target 'stm_vcom.elf' failed

Can you confirm, please?

Thank you.

Jan Waclawek
Visitor II
May 11, 2018 5:35 PM UTC
Posted on May 11, 2018 at 17:35

Examine the mapfile to find out where did the memory go.

JW

David Martins
Senior
May 14, 2018 1:49 PM UTC
Posted on May 14, 2018 at 15:49

Now I can compile the code, but my windows PC still does not detect the device, as USB COM port.

This is my circuit and I think everything is correct to work ...

Could it be a Drivers problem?

https://s7.postimg.cc/xyfqthd7v/Capturar.png

Khouloud GARSI
ST Employee
May 16, 2018 12:55 PM UTC
Posted on May 16, 2018 at 12:55

Hi Martin,

  • Now I can compile the code,

-> Could you please share the encountered issue and the solution. This will be helpful for other STM32 MCUs users who are  facing the same issue.

  • Are you building a bus or self powered USB application?

Khouloud.

David Martins
Senior
May 16, 2018 1:10 PM UTC
Posted on May 16, 2018 at 13:10

garsi.khouloud

‌,

I already explained how I managed to compile. Did you see this post?

https://community.st.com/0D50X00009XkeFHSAZ

Change the APP_RX_DATA_SIZE and the APP_TX_DATA_SIZE to 64 solve the problem.

Can you confirm that it is

a CubeMX bug?

This is the circuit I have on my PCB:

https://community.st.com/0D50X00009XkeFHSAZ

All power comes from USB (J2 - is the USB connector).

David Martins
Senior
May 16, 2018 10:54 AM UTC
Posted on May 16, 2018 at 12:54

This forum is being watched?

Any news? Some help?

Nawres GHARBI
ST Technical Moderator
May 18, 2018 8:44 AM UTC
Posted on May 18, 2018 at 10:44

Hi David, 

The user tags have been kept for compatibility with old project where the RX and TX buffer size weren't generated bu CubeMX. 

2048 will never be compiled as your chip is of 6KByte RAM (0x1800), you have to set a lower value that fits in your RAM