Skip to main content
Associate II
Aug 11, 2025 11:39 PM UTC
Question

STM32CubeWBA V1.7.0 – New UTIL timer used for HAL tick increment in MX_APPE_Init()

 

After updating to STM32CubeMX 6.15.0 with STM32CubeWBA FW V1.7.0 for the STM32WBA63CIUx, I noticed a change in how the HAL tick is driven.

In MX_APPE_Init() (generated in app_entry.c), CubeMX now creates a UTIL timer to increment the HAL tick:

 /* Create an RTC based timer to trigger HAL tick increment */
 UTIL_TIMER_Create(&TimerHALtick_Id,
 HAL_TICK_FREQ_100HZ,
 UTIL_TIMER_PERIODIC,
 &TimerHALtickCB, 0);
 uwTickFreq = HAL_TICK_FREQ_100HZ;

 /* Start HAL tick timer */
 UTIL_TIMER_StartWithPeriod(&TimerHALtick_Id, HAL_TICK_FREQ_100HZ);

This runs at 100 Hz by default and causes my system to wake every 10 ms.

Previously, I used TIM17 for the HAL tick, with FreeRTOS (tickless idle) and STM32_WPAN BLE, and it worked well. Now, I see both TIM17 and this new UTIL timer, which leads to unnecessary wakeups.

My questions:

  1. Is there official documentation on this new HAL tick implementation using UTIL_TIMER?

  2. How can it be configured or disabled via STM32CubeMX instead of modifying the generated code?

  3. If I want a 1 ms HAL tick, should I reconfigure the UTIL timer to 1000 Hz, or simply disable it and keep using TIM17?

  4. What is the intended use case for this change in FW V1.7.0?

I could not find any CubeMX option to select between TIM17 and this UTIL timer. Any guidance or reference to documentation would be appreciated.

 

 

This topic has been closed for replies.

4 replies

STTwo-32
ST Technical Moderator
Aug 12, 2025 9:29 AM UTC

Hello @lgc 

Could you please add the .ioc file you have createed.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
lgcAuthor
Associate II
Aug 12, 2025 2:09 PM UTC

Hello @STTwo-32, I attached the migrated .ioc file. Thank you.

lgcAuthor
Associate II
Aug 18, 2025 4:34 PM UTC

Hello @STTwo-32 , is there an update on this topic?

Thanks and regards

lgcAuthor
Associate II
Aug 26, 2025 7:04 PM UTC

Hello, just a friendly reminder about this topic. Is this being looked at by someone?