Skip to main content
kurta999
Senior
Feb 26, 2019 7:50 PM UTC
Solved

STM32CubeMX5.1.0 ADC "DMA Continuous Requests" doesn't work

I opened an older project which was created with 5.0.1, and the newest CubeMX shows an error for this option in ADC. But this option is correct. I tried to create a new project, and I wasn't able to enable this option here.

This topic has been closed for replies.
Khouloud ZEMMELI
Khouloud ZEMMELIBest answer
ST Employee
Mar 1, 2019 3:35 PM UTC

​Hello @kurta999​ 

You are right , Issue will be fixed in the next CubeMX release.

Best regards,

Khouloud

33 replies

mospi
Visitor II
Aug 7, 2019 4:44 PM UTC

This is the ioc

Thanks

SAkht
Visitor II
Sep 19, 2019 8:00 AM UTC

Same problem here with STM32F446RE. No DMA continously request available.

STM32CubeIDE version 1.0.2 Build: 3566_20190716-0927 (UTC)

wiht

STM32CubeMX version 5.3.0. Build: 20190711-0903 (UTC)

STM32F401RE is working with same versions.

HJung.6
Associate II
Oct 29, 2019 6:12 AM UTC

same problem. it make me crazy!! very angry!!​

Khouloud ZEMMELI
ST Employee
Oct 29, 2019 8:33 AM UTC

Issue already fixed, You have a missed  config  in your project.

Please  Add " DMA Request " under DMA Settings .

Regards,

Khouloud.

JWhit.7
Visitor II
Jul 14, 2020 10:56 PM UTC

I'm using STM32CubeIDE v1.3.1 and am experiencing the same issue with a STM32F469 board. I've attached the ioc.

Khouloud ZEMMELI
ST Employee
Jul 17, 2020 2:27 PM UTC

​Hi @JWhit.7​ , I'll check it.

Regards,

Khouloud

Khouloud ZEMMELI
ST Employee
Jul 17, 2020 2:37 PM UTC

​you're right, the 6.0.0 will be available for the next week, it's OK on 6.0.0.

We are deeply sorry for any inconvenience this may have caused.

Regards,

Khouloud