Skip to main content
robertbocquier9
Associate
Aug 19, 2014 9:25 AM UTC
Question

STM32CubeMX won't configure PA7

Posted on August 19, 2014 at 11:25

Hi all,

I am trying to configure a STM32F302VBTx using STM32CubeMX, and I am experiencing a strange behavior with ADC2/IN4 (PA7).

Steps to reproduce:

  • create a new project
  • picks STM32F302VBTx
  • enable ADC2 IN3 as single ended (uses PA6)
  • enable ADC2 IN4 as single ended (uses PA7)
  • go to configuration, System, GPIO
  • look at GPIO mode: PA6 is marked as ''Analog mode'' (which is expected), but PA7 is listed as ''n/a''
  • click on PA7 row, a warning says ''There are no parameters to be configured'' (while again PA6 works as expected)

Is it true that PA7 is somewhat special?

Is this a bug in STM32CubeMX database?

Thanks for any advice

#stm32cubemx
This topic has been closed for replies.

4 replies

stm32cube-t
ST Employee
Sep 10, 2014 9:18 AM UTC
Posted on September 10, 2014 at 11:18

Hello Robert,

This issue has been fixed for the next STM32CubeMX release: 4.4.

Best regards

Charles Miller
Associate III
Oct 11, 2014 3:20 AM UTC
Posted on October 11, 2014 at 05:20

STM32Cube-T, the Release notes are still at 4.3 on the cube download page.

Regards,

Chuck

Charles Miller
Associate III
Oct 11, 2014 3:45 AM UTC
Posted on October 11, 2014 at 05:45

Actually, the label says ''4.4.0'', but the .zip file contains 4.3.1.

Server didn't get updated?

Amel NASRI
ST Technical Moderator
Oct 15, 2014 9:00 AM UTC
Posted on October 15, 2014 at 11:00

Hi Charles,

The CubeMX release published on the web isn't the official one. Issue will be fixed soon. 

Sorry for such inconvenience.

-Mayla-

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.