Skip to main content
Associate II
Sep 25, 2023 3:58 PM UTC
Solved

STM32CubeMX with IAR, C++, FreeRTOS and multi-thread support - hanging in startup before main

STM32CubeMX 6.9.1 and IAR 9.32.1 on Nucelo_L476RG

When enabling multi-threaded support for our FreeRTOS project in STM32CubeMX I am seeing builds of the binary that during startup (before reaching main) there are calls to __iar_system_Mtxlock() (dlib_lock_glue.c) before __iar_system_Mtxinit() and as the locks are not initialised, the system hangs in Error_Handler().

Is there anything I need to do to do in startup for this to work correctly?

This topic has been closed for replies.
hbucknellBest answer
Associate II
Nov 30, 2023 4:55 PM UTC

Hello ST,

I have fixed this with support from IAR. dlib_lock_glue.c from STM32CubeMX is at fault.

ST: please can you update the dlib locking code as generated in CubeMX?

 

To fix this issue requires the following steps,

  1. Linker -> Extra Options ->  --manual_dynamic_initialization
  2. Refactor "__attribute__ ((constructor)) void __dlib_thread_safety_init()" to "void __dlib_thread_safety_init()"
  3. Early in main(), beofre any C++ code is called,
    1. Declared “extern void __dlib_thread_safety_init();”
    2. Called the following at the beginning on main,
    3.     __dlib_thread_safety_init();
    4.     __iar_cstart_tls_init(NULL);
    5.     __iar_dynamic_initialization();

Also, the mutex lock/unlock functions in dlib_lock_glue are wrong, the ones generated for the STM32CubeIDE are correct, but the IAR ones are out-of-date.

References to "static_system_list_lock" and "static_file_list_lock" in the following functions (and only the following functions) should be deleted/commented out,

  • __iar_system_Mtxlock
  • __iar_system_Mtxunlock
  • __iar_file_Mtxlock
  • __iar_file_Mtxunlock

I hope this helps someone facingteh same issues we have been facing.

H.

9 replies

hbucknellAuthor
Associate II
Sep 25, 2023 4:17 PM UTC

It appears that __dlib_thread_safety_init() is not being called. As this is where __iar_Initlocks() is called from. Still invetigating.

hbucknellAuthorBest answer
Associate II
Nov 30, 2023 4:55 PM UTC

Hello ST,

I have fixed this with support from IAR. dlib_lock_glue.c from STM32CubeMX is at fault.

ST: please can you update the dlib locking code as generated in CubeMX?

 

To fix this issue requires the following steps,

  1. Linker -> Extra Options ->  --manual_dynamic_initialization
  2. Refactor "__attribute__ ((constructor)) void __dlib_thread_safety_init()" to "void __dlib_thread_safety_init()"
  3. Early in main(), beofre any C++ code is called,
    1. Declared “extern void __dlib_thread_safety_init();”
    2. Called the following at the beginning on main,
    3.     __dlib_thread_safety_init();
    4.     __iar_cstart_tls_init(NULL);
    5.     __iar_dynamic_initialization();

Also, the mutex lock/unlock functions in dlib_lock_glue are wrong, the ones generated for the STM32CubeIDE are correct, but the IAR ones are out-of-date.

References to "static_system_list_lock" and "static_file_list_lock" in the following functions (and only the following functions) should be deleted/commented out,

  • __iar_system_Mtxlock
  • __iar_system_Mtxunlock
  • __iar_file_Mtxlock
  • __iar_file_Mtxunlock

I hope this helps someone facingteh same issues we have been facing.

H.

hbucknellAuthor
Associate II
Nov 11, 2024 2:49 PM UTC

There have been a few other minor updates, but here are the files I am now using in case it helps anyone else.

Graduate
Nov 11, 2024 2:59 PM UTC

Thank you very much for your answer. Much like the STM boilerplate code, the messaging is falling apart so I'm answering to you here.

unfortunately, there is some other error elsewhere:

void __iar_file_Mtxinit(__iar_Rmtx *lock)

 

It says that there are not enough Mutexes. I'll have to take this with IAR support.
But thank you very much anyways!

Kind regards,
Nikola

hbucknellAuthor
Associate II
Nov 11, 2024 3:06 PM UTC

Hi Nikola, I believe you can change the number in the stm32_lock.h file, line 256

Graduate
Nov 12, 2024 8:23 AM UTC

Thank you so much ! I will try it out ..maybe it'll help.