Skip to main content
Associate
Apr 7, 2026 8:22 PM UTC
Solved

STM32CubeMX Version 6.16 HRTIM problems Nucleo G474RE

After updating CubeMX to version 6.16.2, we are seeing HRtimer E and F problems which cause our product to fail.  Reverting back to 6.15 and regenerating the code allows our device to work.  I believe the issue is due to the change in the code database version: MxDb.Version=DB.6.0.161 but I can't be sure as the new version of cubeMX forces values into the HRtimer E and F configurations.

Hoping for commiseration and resolution!

Thanks

Rauk

Souhaib MAZHOUDBest answer
ST Technical Moderator
Jul 3, 2026 1:44 PM UTC

Hello @raulatkinson 

This issue has been fixed in the latest version of STM32CubeMX 6.18.0 

Download STM32CubeMX6.18.0 from this link. 

Regards,

Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

8 replies

TDK
Apr 7, 2026 8:24 PM UTC

Do a diff of your codebase before/after the change to find the actual code differences. There are release notes as well but comparing the code would be more precise.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate
Apr 7, 2026 11:59 PM UTC
Yes, Thank you!

I did that. There are over 40 files that changed. Many of these are line
ends or other whitespace modifications, but some are more suspicious
looking:


--- a/Drivers/STM32G4xx_HAL_Driver/Src/stm32g4xx_hal_hrtim.c
+++ b/Drivers/STM32G4xx_HAL_Driver/Src/stm32g4xx_hal_hrtim.c
@@ -5087,9 +5087,6 @@ HAL_StatusTypeDef
HAL_HRTIM_WaveformTimerControl(HRTIM_HandleTypeDef *hhrtim,
/* Configure timing unit */
HRTIM_TimingUnitWaveform_Control(hhrtim, TimerIdx, pTimerCtl);

- /* Force a software update */
- HRTIM_ForceRegistersUpdate(hhrtim, TimerIdx);
-
hhrtim->State = HAL_HRTIM_STATE_READY;

/* Process Unlocked */
@@ -9309,9 +9306,13 @@ static void
HRTIM_TimingUnitWaveform_Config(HRTIM_HandleTypeDef *hhrtim,
hrtim_timfltr &= ~(HRTIM_FLTR_FLTLCK);
hrtim_timfltr |= pTimerCfg->FaultLock;

- /* Enable/Disable dead time insertion at timer level */
- hrtim_timoutr &= ~(HRTIM_OUTR_DTEN);
- hrtim_timoutr |= pTimerCfg->DeadTimeInsertion;
+ /* The deadtime cannot be used simultaneously with the push-pull mode */
+ if (pTimerCfg->PushPull == HRTIM_TIMPUSHPULLMODE_DISABLED)
+ {
+ /* Enable/Disable dead time insertion at timer level */
+ hrtim_timoutr &= ~(HRTIM_OUTR_DTEN);
+ hrtim_timoutr |= pTimerCfg->DeadTimeInsertion;
+ }
I've not had time yet to go through all the possible places for errors


ST Technical Moderator
Apr 8, 2026 2:00 PM UTC

Hello @raulatkinson 

Could you provide your ioc in order to investigate the issue?

BR, Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Associate
Apr 9, 2026 10:48 PM UTC

Looks like I have to put the files here, not as attachments:

ST Technical Moderator
Apr 13, 2026 4:07 PM UTC

Hello @raulatkinson 

After checking your IOC, it seems that you are facing the same issue posted in this thread: Solved: HRTIM configuration when updated to 6.16.1 CubeMX - STMicroelectronics Community.
this behavior is under investigation by the dedicated team, and a fix will be implemented in the upcoming releases.

BR, Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Associate
Apr 13, 2026 5:38 PM UTC

Thank you very much for your response.
Will the fix for this be announced?  I'd like to be notified.
-Raul Atkinson