Skip to main content
Tom Moulton
Associate III
Aug 7, 2018 7:49 PM UTC
Question

STM32CUBEMX Ver 4.26.1 horrific bug

Something has change with Version 4.26(.1)

Any time I look at the Project Settings (even with no changes) I get a message saying:

"This Project File (System.ioc) already exists in the chosen folder. Overwrite this file by this new Project?"

If I say No and I generate code I get an error that the code was generated but the project generation got an error

If I say yes it them proceeds to delete the *entire* Src and Inc directories and creates fresh files. It even deletes my source files and hidden files (like CVS dir)

Any changes to main.c or ethernetif.c (USER CODE) are totally lost

I am using Atollic 9.0 (TrueSTIDIO project format)

My processor is the STM32F407

What triggers Cube to think I am creating a new project?

WHY does Cube think it is OK to delete files it knows nothing about?

Tom

This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
Aug 7, 2018 11:01 PM UTC

>>WHY does Cube think it is OK to delete files it knows nothing about?

I think it significantly simplifies the implementation.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Grisby
Associate II
Aug 8, 2018 7:57 AM UTC

I simple clear the whole folder. I also think it is not OK.

Bertrand1
Senior
Aug 8, 2018 10:27 AM UTC

I had also this. Incredible to have no warning before deleting external files.

Tesla DeLorean
Guru
Aug 8, 2018 1:08 PM UTC

The first rule of automated code generation tools is to run them in a sand-box, especially ones you use iteratively. It is not a matter of IF they will fail, but WHEN.

Use a merge tool to pull into the trees you have under a source code control system.

Yes the implementation here is horrific, but we've been talking about it for YEARS

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..