Skip to main content
JPan.4
Associate II
Mar 20, 2024 5:43 PM UTC
Solved

STM32CubeMX V6.11.0: Migration issue - ADC3 Temperature Sensor Channel missing

Target Board: STM32H743ZI2 Nucleo

STM32CubeMX: V6.11.0

 

Hallo community,

I'm encountering an issue about migration. When I migrated my STM32CubeMX project from V6.10.0 to V6.11.0, the setting for ADC3 was disabled in the new *.ioc files. In my old ADC3 settings, I was using the Temperature Sensor Channel on the chip. But after the update to V6.11.0, the setting for Temperature Sensor Channel in the ADC3 is missing. All the settings of ADC3 for the temperature sensor are missing, and there is no ADC channel 18 under ADC3 to set (The inner temperature sensor is connected to ADC channel 18).

I've also checked the STM32CubeMX 6.11.0 release note and errata. There is no such an issue reported.

I put the two screenshots in the attached files.

 

Best wishes,

 

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Mar 21, 2024 7:59 AM UTC

Hello,

The internal ticket 176638 (not accessible by the community users) has been created to confirm/fix the issue.
So please follow the news on this thread here as stated by @Peter BENSCH 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

4 replies

STTwo-32
ST Technical Moderator
Mar 20, 2024 6:24 PM UTC

Hello @JPan.4 

Thank you for reporting this. I will escalate it intenally to the concerned team for more investigation.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Peter BENSCH
ST Technical Moderator
Mar 20, 2024 6:44 PM UTC

Essentially the same problem as here.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Mar 21, 2024 7:59 AM UTC

Hello,

The internal ticket 176638 (not accessible by the community users) has been created to confirm/fix the issue.
So please follow the news on this thread here as stated by @Peter BENSCH 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Associate III
Aug 27, 2024 6:54 AM UTC

HOW TO CONFIGURATION INITILAZTION  GIVE ME INFORMTION ADC3 TEMPRETURE CALCULTION ON THIS CHANNEL