Skip to main content
MaxR
Associate
Sep 14, 2018 7:08 AM UTC
Solved

STM32CubeMX V4.27.0 release note states that STM32H7 uses firmware V1.4.0. Whereas in reality it uses V1.3.0.

STM32CubeMX V4.27.0 release note states that STM32H7 uses firmware V1.4.0. Whereas in reality it uses V1.3.0. Is it possible to download STM32H7 firmware V1.4.0. I could not find it anywhere. Is firmware update planed?

This topic has been closed for replies.
Houda GHABRI
Houda GHABRIBest answer
ST Employee
Sep 18, 2018 9:54 AM UTC

Hello @MaxR​  ,

We are sorry, there is a typo in Release note of STM32CubeMX 4.27.0 , STM32H7 use V1.3.0 and not 1.4.0.

It is not possible to download the H7 FW 1.4.0 because it is not yet available :) but update is planned for the future.

Regards,

Houda

3 replies

Khouloud GARSI
ST Employee
Sep 14, 2018 12:57 PM UTC

Hi @MaxR​ ,

The STM32H7 uses STM32Cube firmware V1.3.0. This is a typo in the release note which will be fixed in the next update of the document.

Thanks for bringing this point to our attention.

Khouloud.

Tesla DeLorean
Guru
Sep 14, 2018 3:43 PM UTC

>>Is firmware update planed?

It is, but there isn't a schedule, and current release supports the NUCLEO/EVAL boards fully

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Houda GHABRI
Houda GHABRIBest answer
ST Employee
Sep 18, 2018 9:54 AM UTC

Hello @MaxR​  ,

We are sorry, there is a typo in Release note of STM32CubeMX 4.27.0 , STM32H7 use V1.3.0 and not 1.4.0.

It is not possible to download the H7 FW 1.4.0 because it is not yet available :) but update is planned for the future.

Regards,

Houda