Skip to main content
frackers
Senior
Sep 23, 2018 11:49 PM UTC
Solved

STM32CubeMX v4.27.0 can't disable Scan Conversion Mode on ADC of F4

As in the title, I've just updated to 4.27.0 and it insists on enabling Scan Conversion mode. This causes my ADC code to fail.

Since there are no alternate options, why is the item in the menus?

This topic has been closed for replies.
frackers
frackersBest answer
Senior
Oct 10, 2018 12:43 AM UTC

SOLVED!!

If more than 1 ADC channel is selected such that "Number of Conversion" is > 1 then the scan mode is turned on automagically. Since I'm selecting the inputs individually and not scanning I just have to make sure I DON'T set them all up in CubeMX

2 replies

ST Technical Moderator
Sep 24, 2018 10:52 AM UTC

Hello @frackers​ ,

After check, I can disable Scan Conversion Mode on ADC for STM32F4 using STM32CubeMx version 4.27.0

0690X000006C4TYQA0.jpg

Please share your ioc file for check your case.

With Regards,

Imen.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
frackers
frackersAuthorBest answer
Senior
Oct 10, 2018 12:43 AM UTC

SOLVED!!

If more than 1 ADC channel is selected such that "Number of Conversion" is > 1 then the scan mode is turned on automagically. Since I'm selecting the inputs individually and not scanning I just have to make sure I DON'T set them all up in CubeMX