Skip to main content
JOsen
Associate II
March 12, 2019
Solved

STM32CubeMX used to configure a CAN channel on stm32f4-discovery

  • March 12, 2019
  • 2 replies
  • 1042 views

New to STM32CubeMX. I am using a stm32f4-discovery. I want to use a CAN channel. It seems that the external memory may be blocking me.

Is there a way to get a CAN channel available for this dev board?  

I would like to end up with the LCD + UART + CAN. I hope there is a lighter weight LCD library that will let this happen in the 2MB of STM32 FLASH and avoid the external FLASH.

This topic has been closed for replies.
Best answer by JOsen

STM32F469I DISCO seems to have a CAN channel that can be configured.

2 replies

JOsen
JOsenAuthor
Associate II
March 17, 2019

I remembered that I have a STM3210C-Eval available. It has a CAN channel available and configured. I will use that.

This thread can be closed.

JOsen
JOsenAuthorBest answer
Associate II
February 22, 2020

STM32F469I DISCO seems to have a CAN channel that can be configured.