Skip to main content
dhaselwood
Associate III
Oct 27, 2021 4:35 PM UTC
Solved

STM32CubeMX: STM32L431RC: ADC IN14 has incorrect conflict message

With my pin assignments ADC IN14 shows a conflict with PB0. Which is incorrect according to the datasheet. The conflict should be with PC5. IN15 also shows a conflict with PB0 which is correct.

This topic has been closed for replies.
TDK
TDKBest answer
Oct 31, 2021 1:16 AM UTC

The warning on IN14 is saying you can't enable differential mode because IN15/PB0 is occupied. If there were a conflict with PC5, you wouldn't be able to enable single-ended mode either. No bug here.

"If you feel a post has answered your question, please click ""Accept as Solution""."

4 replies

TDK
Oct 27, 2021 4:53 PM UTC

Please show a screenshot and/or include the IOC file.

"If you feel a post has answered your question, please click ""Accept as Solution""."
dhaselwood
Associate III
Oct 31, 2021 1:09 AM UTC

Attached is the ioc file.

TDK
TDKBest answer
Oct 31, 2021 1:16 AM UTC

The warning on IN14 is saying you can't enable differential mode because IN15/PB0 is occupied. If there were a conflict with PC5, you wouldn't be able to enable single-ended mode either. No bug here.

"If you feel a post has answered your question, please click ""Accept as Solution""."
dhaselwood
Associate III
Nov 1, 2021 6:13 PM UTC

I suggest adding some words to the message that indicates that the conflict is with the differential mode.