Skip to main content
Jack3
Senior
May 3, 2019 9:48 AM UTC
Question

STM32CubeMX / STM32CubeIDE100 - Recommendations

In the build-in CubeMX, there are some improvements possible:

  • Unable to alter some pull-down boxes in the Clock Configuration, they disappear when trying to move the mouse to the desired selection (must use cursor and enter keys instead)
  • When selection a GPIO or Peripheral from the menu at the left, high-light the associated pins on the chip package
  • When clicking "Enter User Label" on a pin on the Pinout view, automatically place the cursor in the input field (focus)
  • If LWIP is disabled (it can not be enabled) explain why it is disabled, and/or offer to change the minimum requirements (like DCache enable)

I don't know if ST checks these kind of posts.

Maybe other users can contribute as well.

This topic has been closed for replies.