Skip to main content
Associate
Jul 30, 2026 7:48 PM UTC
Question

STM32CubeMX project works after generation but fails after reopening

Hi everyone,

I’m working on an STM32 project using STM32CubeMX and STM32CubeIDE. Everything builds and runs correctly right after generating the project, but after closing and reopening the project I sometimes run into build errors related to generated files or missing libraries.

Regenerating the code usually fixes it, but I’m trying to understand why this happens in the first place.

Has anyone experienced something similar with CubeMX projects? Is there a recommended way to organize the project or CubeMX settings so that generated files and middleware remain consistent when reopening the project?

I’d appreciate any advice or best practices from people who work with STM32CubeMX regularly.

2 replies

Visitor II
Jul 30, 2026 9:08 PM UTC

I've seen this happen a couple of times, and in my case it usually wasn't the generated code itself. A few things that are worth checking:

  • Make sure the .ioc file stays in the project root and is committed if you're using version control.

  • After reopening the project, try Project → Clean and then rebuild before regenerating code.

  • Verify that the project is still using the same STM32Cube firmware package version that it was generated with. If CubeMX or CubeIDE switches to a different firmware version, generated middleware files can change unexpectedly.

  • If include paths or linked resources are missing, right-click the project and choose Refresh, then check the project properties to confirm the include paths are still present.

If regenerating always fixes the issue, there's a good chance the problem is related to the project metadata or the IDE workspace rather than your application code.

Out of curiosity, what are the actual build errors you're seeing after reopening? The first error in the build log usually points to the real cause. That would make it much easier to narrow down whether it's a missing include path, firmware package mismatch, or something else.

Amnguspro.com
Associate
Jul 31, 2026 5:01 PM UTC

Thanks, that’s really helpful. I hadn’t checked the firmware package version and project metadata closely enough. I’ll compare those and look at the first build error after reopening. Appreciate the pointers!