Skip to main content
SKape
Associate II
Mar 18, 2019 4:00 PM UTC
Question

STM32CubeMX project generation have problem BUG on samba

​Hello.

I work on Windows on a network drive.

The file server is samba which, by default, for files whose name starts with a dot, gives the hidden attribute.

After generating the TrueStudio project, the .project and .cproject files are thus given a hidden attribute.

When re-generating the project using CubeMX, the following error appears: '' The Code is fully generated under (mypathname), but TrueSTUDIO project generation have a problem. ''

I can not change file server settings, therefore I am unable to remove the attribute hidden from the .project and .cproject file.

Is it possible the STM32CubeMX will work with the TrueSTUDIO project files that have hidden attributes?

This topic has been closed for replies.