Skip to main content
nicholas
Associate II
Mar 6, 2014 12:02 PM UTC
Question

STM32CubeMX Project files for STM324xG-EVAL

Posted on March 06, 2014 at 13:02

Hi,

It would be great to have access to the STM32CubeMX project files for various evaluation and demonstration boards, like the STM324xG-EVAL that uses the STM32F407IGH6 processor. This would greatly help porting a dev board to a custom PCB.

Thanks,

Nicholas

#stm32cubemx #stm324xg-eval
This topic has been closed for replies.

8 replies

frankmeyer9
Associate III
Mar 6, 2014 12:59 PM UTC
Posted on March 06, 2014 at 13:59

As I understood it, everthing that is finished yet is also available for download.

Just check the appropriate ST website.

So what you are looking for might still be in the making.

Would be great if some ST guys could enlighten us about the release roadmap ...

Tesla DeLorean
Guru
Mar 6, 2014 1:24 PM UTC
Posted on March 06, 2014 at 14:24

Like STM32Cube_FW_F4_V1.0.0\Projects\STM324xG_EVAL\Examples\ADC\ADC_TriggerMode\MDK-ARM\Project.uvopt or what specifically?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
nicholas
nicholasAuthor
Associate II
Mar 6, 2014 2:41 PM UTC
Posted on March 06, 2014 at 15:41

Hi Clive1,

No... ST has made a rather nice configuration manager called STM32CubeMX. I want the project file for the various dev boards - so it will be something like:

STM324xG-EVAL.ioc

which I can then use to see the pin mappings, clock settings, etc. and obviously change these to my specific needs.

nicholas
nicholasAuthor
Associate II
Mar 7, 2014 8:16 AM UTC
Posted on March 07, 2014 at 09:16

Hey Clive1,

That is exactly what I was looking for... but hoped for the STM324xG-EVAL version.

Thanks,

Nicholas

miltonhotard
Visitor II
Mar 18, 2014 3:18 PM UTC
Posted on March 18, 2014 at 16:18

I am looking for the same thing as you. No luck yet?

nicholas
nicholasAuthor
Associate II
Mar 26, 2014 7:36 AM UTC
Posted on March 26, 2014 at 08:36

Nope! Seems we need to wait for ST...

stm32cube-t
ST Employee
Jun 5, 2014 3:36 PM UTC
Posted on June 05, 2014 at 17:36

Hello,

Using STM32CubeMX v4.2 you can now select an ST Board instead of only an MCU when starting a new project. Additional boards will be supported with the version 4.3 coming out few weeks from now.

Best Regards