Skip to main content
Associate
Nov 5, 2026 9:26 AM UTC
Question

STM32CubeMX - Power Consumption Calculator - no Peripheral consuption in SMPS mode

Hi there,

 

I’m working with STM32CubeMX 6.18.1 and try to estimate the power consumption for a STM32H5F4ZJTxQ.

After trying different combinations I found that the consumption of the peripherals is not calculated if an SMPS-Mode is selected in the PowerScale dropdown box.

For example if “VOS0: Scale 0” is selected, the Result shows 27,05mA for the peripherals in my configuration. When I switch to “VOS0: Scale 0/SMPS” and leave the other parameters as before, the Result shows 0 nA for the peripherals.

27,05mA without SMPS

 

0 nA with SMPS

Am I missunderstanding something or is this a bug in the calculation tool?

Regards, Peter 

 

1 reply

ST Technical Moderator
Nov 5, 2026 9:51 AM UTC

Hello ​@PowerStation 

Thank you for reporting this issue.

Could you provide an IOC that illustrates the issue in order to investigate further?

KR, Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.