Associate III
Dec 24, 2016 8:51 PM UTC
Solved
STM32CubeMX on UHD (4K) display - clock configuration diagram too small to see
- 24 replies
- 8766 views
Posted on December 24, 2016 at 21:51
Using STM32CubeMX version 4.18.0 on Windows 10 Pro (build 1607) with an UHD (4K) display results in tiny toolbar icons and a very tiny Clock Configuration diagram. Please see attached screen capture image. Not that this application window is not maximized.
Is there any way to scale these images within the STM32CubeMX application so that I can see them with human eyes?
Additionally, the screen looks the same even when I drag the STM32CubeMX application to a different, lower-resolution monitor.
Any help would be appreciated.
Thanks,
Dale
#stm32cubemx