Skip to main content
Rickta59
Visitor II
July 27, 2018
Question

STM32CubeMX on linux generates a call to arm-none-eabi-objcopy.exe which doesn't exist

On linux if I use the latest STM32CubeMX (4.26.1) and generate a project for Atollic Truestudio, the project tries to use the executable called 'arm-none-eabi-objcopy.exe' this is the name for the windows verison however on linux it is called 'arm-none-eabi-objcopy' without the extension.

If I fix the project setting and save, the next time I use STM32CubeMX on the same project and regenerate it wipes out my change.

This topic has been closed for replies.

2 replies

Amel NASRI
ST Technical Moderator
August 3, 2018

Thanks @Rickta59​  for reporting this issue. It will be reviewed by our STM32CubeMX experts.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
Mohamed Mansouri
Visitor II
August 9, 2018

Hi Rickta59,

Thanks for your feedback.

I confirm that it is a bug and it will be fixed next release.

Please do not hesitate to contact me for further details.

Thanks and regards,

Mohamed

,

Thanks for your feedback.

I confirm that it is a bug and it will be fixed next release.

Please do not hesitate to contact me for further details.

Thanks and regards,

Mohamed