Skip to main content
michaelkotthaus9
Associate III
Mar 21, 2017 5:48 PM UTC
Question

STM32CubeMX: missung initialization of Rx and Tx pins

Posted on March 21, 2017 at 18:48

Hi STM32 Support Team,

I have an existing STM32CubeMX project for the Nucleo-F303RE board which uses UART2. In the project the pins PA2 (Tx) and PA3 (RX) are configured as alternate function pins. In the old code (probably generated with V4.x) I could see that the pins were correctly initialized, file main.c, function MX_GPIO_Init:

 /*Configure GPIO pins : USART_TX_Pin USART_RX_Pin */
 GPIO_InitStruct.Pin = USART_TX_Pin|USART_RX_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF7_USART2;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);�?�?�?�?�?�?�?

Now, I am using a newer version of STM32CubeMX (V.4.0 and also newer libraries) and the above mentioned code is missing! Also, the TX pins is showing a low level in idle state. (I would have expected a high level.)

Can you confirm this issue? Is this an intentioned feature?

Regards,

michaeL

PS at developmentteam: I would be very helpful if you would enclose in all auto-generated fils which STM3CubeMx was used and which libraries were involved.

#uart #stm32cubemx
This topic has been closed for replies.

5 replies

ST Technical Moderator
Mar 22, 2017 8:40 AM UTC
Posted on March 22, 2017 at 09:40

Hello michaeL , 

Please share your .ioc file, I will report internally your issue for further check.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
michaelkotthaus9
Associate III
Mar 22, 2017 11:21 AM UTC
Posted on March 22, 2017 at 11:21

Hello

DAHMEN.IMEN

‌,

I just uploaded theIOC file to

https://community.st.com/servlet/JiveServlet/downloadBody/1418-102-1-1712/UART_test.ioc.zip

.

When I generate code with STM32CubeMX V4.20 in the file main.c the above code snippet is missing.

michaeL

ST Employee
Jul 6, 2017 4:29 PM UTC
Posted on July 06, 2017 at 16:29

Hello

Kotthaus.Michael

,

I would like to thank you for your feedback.

I used a CubeMX4.1 to reproduce your symptoms, and the only way to have the code you mention, is to select the F303 SoC, and select PA2 and 3 as USART2_TX and RX, modify the label with USART_TX and RX, and then the GPIO code is generated as following:

/*Configure GPIO pins : USART_TX_Pin USART_RX_Pin */

GPIO_InitStruct.Pin = USART_TX_Pin|USART_RX_Pin;

GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;

GPIO_InitStruct.Alternate = GPIO_AF7_USART2;

HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

Which is the same as your.

But doing this, the UART IP initialisation is not generated.

I test with latest cube version (ver 4.21) and I can generate the same code

If you want to generate the UART initialisation code, you have to select it in the IP list.

But then the gpio init code will not be generated.. they are exclusive.

To have the high level, I guess you have to configure the pull-up in GPIO configuration panel, go under GPIO Settings tab and select pull-up.

Hope it help

Kind regards

Sirma