Skip to main content
nadiradn
Visitor II
Oct 7, 2015 6:19 AM UTC
Question

STM32CubeMX Issues

Posted on October 07, 2015 at 08:19

have you ever noticed, that pinout and clock config tabs aren't matching each other?

especially if you select Nucleo or Discovery Boards, on pinout Tab you can see pin's selected and marked properly, but Clock configuration tab doesn't reflect proper crystals ...

for STM32F4 Discovery there is an issue with clocking ratios so when you move to clock config tab mostly it is red overclocked... 

for STM32F466RET Nucleo board, it doesn't reflect 32 kHz crystal connected to the MCU PC14,PC15...

 

#stm32 #cubemx
This topic has been closed for replies.

2 replies

Nickname5522_O
Visitor II
Oct 7, 2015 3:02 PM UTC
Posted on October 07, 2015 at 17:02

Hi nadiradze.nikoloz,

Which version of CubeMx are you using?

-Shahrzad-

aaron239955_stm1_st
Senior
Oct 9, 2015 11:50 PM UTC
Posted on October 10, 2015 at 01:50

Yes, I did notice that in an old version of the tool.  Download the current versions of CubeMX and the F4 modules and the clock tree is correct.