Skip to main content
Associate II
January 14, 2026
Solved

stm32cubeMX is not starting

Hello,

I was using STM32CubeMX, but starting two days ago, when I launch the program, only the splash screen appears and the STM32CubeMX does not proceed any further.

1. I have tried deleting the program, restarting the computer, reinstalling it, and running it again.
2. Adding a new user is not possible; the user creation permission is restricted to the company's IT administrator.

I would appreciate any suggestions on additional steps I could take to resolve this issue.

Pavel A.
Pavel A.Best answer
January 15, 2026

You wrote about restrictions by the company's IT administrator. Have they installed some "security", "compliance" and so on software? These things can be intrusive and affect Java applications. More to this, they are managed remotely and can change behavior without any update of the user's software. Can you ask the IT administrator to disable this stuff?

 

9 replies

Ozone
Principal
January 14, 2026

You should at least note the OS you are working with, and the CubeMX version.

Under Unix/Linux, starting an application from commandline usually yields the error messages you are looking for. Not sure about Windows here ...
Another option is to locate the CubeMX executable, and look for log files created for each start.

Ghofrane GSOURI
ST Technical Moderator
January 14, 2026

Hello @modecs 

As mentioned by @Ozone , we need more informations about your OS and MX version that you are using in order to help you resolve this issue.

THX

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
modecsAuthor
Associate II
January 14, 2026

Hello @Ghofrane GSOURI @Ozone 

OS: Windows 11 Enterprise, 24H2

MX version: I tried ver 6.16.1, 6.16.0, 6.15.0 all. but these were not working

 

THX

modecsAuthor
Associate II
January 14, 2026

Additionally, the same issue occurs with the ST MCU Finder program: it also fails to start. For both applications, the splash screen appears, but the programs do not continue launching; in the Task Manager -> background‑process list they are shown as “OpenJDK Platform binary.”

 
 

 

Ozone
Principal
January 14, 2026

> in the Task Manager -> background‑process list they are shown as “OpenJDK Platform binary.”

Because it's a Java application.

While you can try to run it manually from console to review error messages, they all create a quite extensive logfile.
I don't use either, so I can't point you to explicit path names.

Pavel A.
Pavel A.Best answer
January 15, 2026

You wrote about restrictions by the company's IT administrator. Have they installed some "security", "compliance" and so on software? These things can be intrusive and affect Java applications. More to this, they are managed remotely and can change behavior without any update of the user's software. Can you ask the IT administrator to disable this stuff?

 

modecsAuthor
Associate II
January 15, 2026

Hello @Pavel A. 

I contacted our company's IT administrator and requested to check my company's security software, and finally found out that one of the security programs is causing the issue. it appears I will need to use CubeMX within STM32CubeIDE to verify the pinout, and then wait for the security department to fix any changes to the program.

THX